We now have input noise problem. We want to use ADS1258 to measure a thermistor value (R3 value) The schematics is as follows.
Use R3 = 5K to test
And we use AIN6 to sample ADC_VREP, AIN7 to sample THERMO1_B
The following is the adc cnt of AIN6 and AIN7
AIN6:
AIN7:
we found the variation of AIN6 is much smaller than AIN7. Roughly, Adc cnts are 300 v.s. 3600.
For impedance issue ( R3 & R4 values are big at thermistor circuit), we add opamp before input AIN7, but the noise still exist.
We dont know the source of the noise
Something I missed? any advice to improve noises?
BTW, we get the average of 200 samples' values, and the average looks reasonable....
2. Another problem is that there is a case that we get NEGATIVE adc count in data reading even if we use unipolar operation.
for example, from AIN7, we get adc cnt +7862690,+7862690, +7862690, -7262690, 7862690, 7862690
each channel possibly have this scenario..
anyone else report this issue?
thank you
regards,
Ivan