Hi,
I'm using the ADS115 in single shot mode with single ended inputs. The ALERT/RDY pin is configured as toggling to 0 when conversion is completed.
Function works except when the analog input hits GND. (Analog input GND is in the voltage ratings according to the datasheet). I can see why this might happen, the ADC internal logic for RDY pin is still working as a comparator using both the high threshold and low threshold registers. Hitting GND with single ended inputs you end up having either 0xFFFF or 0x0000 as conversion results which are both 'lower' than the low register.
If this is the case it might be good to explain it better in the datasheet, or am I doing something wrong?
Marco