Hi,
If the Fclk of the AFE 512KHz or 2.048MHz is driven externally from the MCU will the internal core generate the additional two clocks/signals required for the respiratory operation or we need to drive even those two(Modulation clock and Blocking signal) also from the MCU.
Regards,
Kishore.