I use the ADS8861 to measure DC-voltages from +5 V to -5 V. I have a reference voltage source which provides 5 V for the REF-pin of the Converter.
In the datasheet on page 9 is described, that the REF-pin has to be decoupled with a 10 µF capacitor. Has it to be decoupled to GND or should the capacitor be in a row between the REF-pin and the reference voltage source?
Thanks for your help.
Best regards,
Andre Wolken