Other Parts Discussed in Thread: ADS1299,
El "Data Rate" se puede modificar o es específico para cada tarjeta??
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
El "Data Rate" se puede modificar o es específico para cada tarjeta??
He respondido a este mensaje en otro hilo.
Is it possible to modify the device's own interface?
The interface is made in LabVIEW
Hello Luz,
You can find all the source code for the EVM (software and firmware) available for download on the EVM's product page.
Brian
Hello R Maria P,
The lead-off detection register configures the integrated lead-off detection circuitry on the ADS1299. The current direction control register toggles the direction of the current for dc lead-off detection. For more information, please refer to the ADS1299 datasheet beginning on page 30.
Regards,
Brian Pisani
Luz,
You can find the source code on the EVM's product page in the "Order Now" table.
Regards,
Brian Pisani
Hello Luz,
The binary for the DSP should be located in the folder "...\ADS1299EEG-FE\fw". We do not have any installed hardware provision on the board to re-flash the processor. The firmware is actually loaded via a bootstrap loader. We do not support firmware changes to the EVM so it may be difficult to get the firmware back to the factory version. I attached the MMB0 schematic for your reference.
Brian
Is it possible to save the firmware project to a more relevant version?
When I try, I have 4 errors: build-938062609,
ADSProLib.tcf, tcof, increase-build.pl
Luz,
I'm sorry but we only provide the code as reference and we don't guarantee that it will build. I know, however, that there are compatibility issues between the different versions of CCS as it relates to building CCS projects. The code for this EVM was likely written in CCS v3 which is no longer available. However, I recommend that if you are intent on building the project, ask the folks in the Compilers Forum to see if they can help you.
Brian