Other Parts Discussed in Thread: ADS1298
Hello. We have a device with ADS1298R in the following configuration:
AVDD = 3.3V
AVSS = GND(0V)
DVDD = 3.3V
VREF = 2.4V (Internal)
Pace buffer = OFF
Vref buffer = ON
Oscillator - external, 2.048Mhz.
I have a trouble to use "internal test" signals. When I select input multiplexer to Test Signal path on a given channel - the result is not correct. It is a rectangle waveform but the amplitude is about 50uV (instead of 2mV). I have tried a lot of combinations with registers without success.
I have a trouble to read on-chip temperature also. In fact all positions of input multiplexer are not working correctly, except of "Normal Electrode" which is working just fine - I'm able to read correctly what I have on the analog input of the chip.
After a days without success, I bought a development kit. In this way a have a possibility to experiment with pin connections, which is impossible on our board (due to BGA package).
What I found is - when I connect TESTP_PACE_OUT1 and TESTP_PACE_OUT2 pins to AVDD - the "internal test" signal amplitude becomes wrong. The temperature and all other internal measurement channels are also wrong. On my board these pins are connected to AVDD, as recommended by data sheet (see below).
But:
1. On table "Pin Function: NFBGA Package" on page 7 in data sheet - unused pins must be connected to AVDD and it is explicative noted exactly for TESTP_PACE_OUTx pins. This is what we have done on our PCB.
2. Due to the "Figure 25. Input Multiplexer Block for One Channel" - When INT_TEST = 1, the TESTP_PACE_OUTx pins are disconnected from the internal multiplexer, so normally the voltage on the pin should not affect the internal measurements (test, temperature, vdd and etc.).
3. The PACE buffer is OFF, so it should not affect the internal measurements.
So what I'm doing wrong? Is it possible that connection of TESTP_PACE_OUTx pins to AVDD affects measurement of internal signals somehow?
Please, I need an urgent answer, since we have a serie of hundreds of boards which are mounted and waiting for firmware implementation of internal tests signals and on chip temperature measurement.