Hello,
I am conducting analysis on below circuit. Having doubt to use 10K pull up for this circuit. Please suggest appropriate pull up resistors.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I am conducting analysis on below circuit. Having doubt to use 10K pull up for this circuit. Please suggest appropriate pull up resistors.
Hello Krunal,
Frequency of operation is about 400KHz, fast mode.
Connection flow as follows, Master to Level shifter which is having 4.7K pull up. Level shifter to 4ADC's here pull ups need to confirm.
Thanks
Hello,
You should be able to use the formula in the application report: http://www.ti.com/lit/an/slva689/slva689.pdf to calculate the pull-up value. You might have to estimate the parasitic capacitance though.
Assuming the parasitic capacitance ~100 pF and the supply = 3.3 V, you might want to start with a 2.2k ohm pull-up and tweak it if required.
May I know the end-application here?
Thanks,
Krunal