Hi ,
I need to integrate the ADC ads127L01 to a tm4c1924 mcu, like as demo board,
and I need to reach the maximum data rate.
Analyzing the demo board schematic the ADC is connected to SSI module number 3
But I observe that each alternate function pin of SSI3 are shorted together,
see in the demo board schematics for example (SSI_clk) PQ0 is together PF3,
I don't know why.
Since I'm drawing a new schematic I have some dubt: how connect the SPI and in whitch manner the ADC is readed by MCU.
Then my question is if is possible receive the firmware source code (or part of it) of demoboard ADS127L01EVM in order to understand
the interfacing to the MCU and the firmware technique to obtain maximum data rate.
I'm planning use SPI and uDMA to do it.
Best Regards
Diego