I am using the ADS8363 with an STM32F407 processor and interfacing to the ADS8363 with the processor’s SPI interface. I have not figured out a way to send twenty clock pulses to the ADS8363, instead I am sending three eight bit bytes to the ADS8363 immediately after pulsing the Convst/Rd high. When I pulse the Convst/Rd high the ADS8363 Busy goes high and stays high for eighteen clock pulses, but the SDOA line always low. Could the problem be related to sending 24 clocks instead of 20 clocks between pulsing the Convst/Rd? Or is something else wrong. I am using the ADS72/8363 eval board. Here is the setup.
J2 is open, M0 and M1 are both high, should be in Mode 4
J5 jumper connects Convst to Rd.
CS is tied low.
Clock = 1.78MHz
No configuration is sent to the ADS8363
Convt/Rd is pulsed with a high pulse 500nS wide followed by 24 clock pulses.
Convt/Rd rise to first clock rise = 920nS