Hi
We have question of ADS1120.
1.
We obtained the following waveform.
Accroding to the datasheet, the PSW would automatically close when the START/SYNC command is sent.
However, PSW seems to close without sending START/SYNC command in the following.
Is this behavior strange?
2.
After power-up, ADS1120 is set to single-shot mode and then do a single conversion.
Does this device enter the power-down mode after a single conversion automatically?
We have to save power consumption with a single data conversion.
BestRegards