Other Parts Discussed in Thread: LMV1032, OPA350
The datasheet for the ADS8329 states that the analog inputs need to be driven by op-amps. It doesn't give any sort of conditions or reasoning for the op-amps and all I have are assumptions.
I was wondering if the inputs could be driven by the LMV1032 mic pre-amplifier since my application requires the part anyway. This would save money, board space, and power; the most important of which are power and space.
If I can drive the inputs of the ADS8329 with the LMV1032, is there anything that should be taken into consideration when connecting the two? (i.e. DC bias)
Thanks in advance,
Chris