Hello to whom it may concern
Our customer has problem that REFIO voltage is abnormal at ADS8568.
REFIO of normal device is 2.5V, but abnormal device is output 5V.
The power sequence at this time is as follows.
(REFIO voltage is abnormal)
#1 : ±12V(HVDD, HVSS) --> 5V(AVDD) --> 3.3V(DVDD)
However, when changing the power sequence to the following, the REFIO became correct voltage(2.5V).
#2 : ±12V(HVDD, HVSS) --> 5 V (AVDD) --> wait for power supply stabilization --> 3.3 V (DVDD)
#3 : 5V(AVDD) --> 3.3V(DVDD) -- > ±12V(HVDD、HVSS)
In both sequence of # 2 or # 3, REFIO became normal.
(Question)
1, Does the REFIO be adversely affected by the power supply sequence?
2, Which power sequence(#2 & #3) do you recommend as a measure to make REFIO normal?
Best regards,
Gk110