Hi,
I'm looking for an ADC that fits my project.
A signal (+-4V) will be measured with a sensor and converted to a digital signal. The ADC resolution should be greater than 20Bit. The signal will lead to a microcontroller
over SPI. It process the signal and send it to a digital and an analog display. The digital display will display the actual value and has a refresh rate of 5Hz and the analog display, which contains a row of LEDs, has a refresh rate of 20Hz. Frequencies like 16 2/3Hz, 50Hz and 60Hz should be filtered out particularly by the ADC. A keypad is available to interact, like setting limits, ranges, etc.. A Speaker is integrated. The system will be powered by batteries and the power consumption should be as low as possible.
Hope you can help me out. Thx a lot