Dear TI Team,
I am using ADS1198 in our design. I have selected Current Source DC lead off method for lead off detection. The register settings are as per below.
WREG LOFF 0x0F // Comparator threshold at 95% and 5%, Current source // DC lead-off
WREG CONFIG4 0x02 // Turn-on dc lead-off comparators
WREG LOFF_SENSP 0xFF // Turn on the P-side of all channels for lead-off sensing
WREG LOFF_SENSN 0xFF // Turn on the N-side of all channels for lead-off sensing
We are facing problem with lead off detection, when all the chest leads V1-V6 & RL lead is disconnected from the patient's body( only RA LA & LL leads are connected to patients body). I have verified this in 2 devices(same hardware), both of these boards are showing different values only for these particular case. as shown below.
|
As shown in above table, the LOFF_SENS values in DEVICE 2 are changing continuesly(0x00, 0x70,0xF6). if any one or all of the Chest leads are connected, along with the RL lead, both the devices are showing the expected result.
The complete results are shown in following table with respect to 2 devices as below.
|
Please, clarify on the following.
- Why both the devices are showing wrong results when only LA, LL, RA are connected to the body ( RL lead and chest leads V1 to V6 disconnected).
- How the Lead off detection for RL lead is depends on the chest leads V1- V6. ( that means if any one or all of the chest leads is connected along with LA, LL, RA lead, I am getting expected result- LOFF_SENSP = 0xFF, LOFF_SENSN = 0x00)
The schematics for the same is attached below.
Thanks and Regards,
Bhairu