Other Parts Discussed in Thread: PCM1690-Q1, , ADS1675
In the design of my current project the ADC (ADS1672) and the DAC (PCM1690-Q1) require different system clock values. In an effort to make things easier I would like both devices to run off the same system clock. The DAC clock is 24.5760 MHz while the datasheet shows the clock at 20 MHz. The datasheet for ADS1672 shows characteristics for the device using a 20 MHz clock but it does not state that that is the maximum clock frequency. Would it be possible to run the ADS1672 at a clock frequency of 24.5760MHz? In my system there will be an FPGA which will have a system clock between 100 MHz to 150 MHz which I would like to use to generate the system clock for the ADC and DAC and one clock source is always better than 2.
Regards,
Mike Lacroix