I am using the ADS1262 on a temperature sensor configured as a wheatstone bridge and am having terrific results so far! There is just one concerning thing that is happening:
Every so often (really rare) there is a spike in the data read. This read error is caught both by the Status Byte and the CRC Byte. In the datasheet it mentions that you should just reacquire the data, however I am very concerned about what is causing this. Do you have any insights? I have attached a figure containing plots of the raw integer returned from the sensor, Status Byte output, CRC returned from chip with Calculated CRC, the difference between. In all plots you can see two spikes.