Tool/software: Code Composer Studio
Hi
I have my own design with ADS1291.
By default DRDY pin has signal, also there is some data on DOUT pin. If i STOP Convertion with making START pin Low DOUT make nothing.
These are only things normal.
The problem is SPI comm. I cant read any thing. Im see signal true at DIN, CLK, CS pins. But no response.
Also i cant make STOP Convertion from registers or by sending SDATAC command. ADS do get register wirte commands.
For example i can see 0x20 0x00 0xFF (dummy for read) on DIN pin, and CLK CS seem fine but no response from DOUT.
-------------------------------------------------
I use internal oscillator.
I tried to make CLK output with Config2 Register CLK_EN but ADS didnt get it. No Clk output. So I think, cant write to registers.
SPI Clk is 480kHz
VSS = GND,
VREFP is 0V ( is it a problem ?? )
VCAP2 = 5.35V
VCAP1 = 1.36V