Hello,
I'm using the ADS124S08 to measure 12 single ended inputs. I'm using the internal 2.5V as references, and because of my signal, I have to use a voltage divider (2 resistors of 10Kohm).
When the analogue pins are floating the ADC measures something, with an oscilloscope I can see that there are 1.5V in the ANX pins, how is that possible if the IDACx are disabled?
If I connect the AN0 to GND to tests, it should measure 0V but that does not happen either beacuse of the current comming out of the ANX pins.
Regards.