Hello,
I'm having trouble using the ADS1299 to obtain an EMG signal. I've soldered it onto a PCB according to the data sheet and double checked if the VREFP - VREFN = 0.5V, but when I turn it on and just run my fingers through the pins, i get absolutely no change in signal output. It's like there is some other noise artifact that is dominating the signal but I don't know what to do from here. Any help is appreciated.
Below is a schematic of my hardware setup:
This is what the signal looks like over 8 channels when using 24x gain, bias signal generation, SRB1 disabled, and SRB2 enabled.The values are scaled to uV using Table 7 in the datasheet. Electrodes aren't connected to anything, just occasionally running my fingers on them during data collection but i'm seeing absolutely no changes in the signal, just this:
-1270.5625,-1275.5022,-1270.8531,-1276.2175,-1268.2156,-1273.1106,-1271.0767,-1273.0883
-1270.5178,-1275.4799,-1270.7413,-1276.128,-1268.2603,-1273.1553,-1271.0095,-1273.0659
-1270.4731,-1275.4799,-1270.6295,-1276.0164,-1268.3049,-1273.1553,-1270.9872,-1273.0659
-1270.5625,-1275.5022,-1270.6967,-1276.1505,-1268.3497,-1273.0883,-1270.9872,-1273.1106
-1270.5625,-1275.4128,-1270.8083,-1276.1505,-1268.2826,-1273.0212,-1270.9425,-1273.0659
-1270.6072,-1275.3235,-1270.652,-1276.128,-1268.1709,-1273.0883,-1270.9648,-1273.0659
-1270.5625,-1275.301,-1270.6743,-1276.1952,-1268.2156,-1273.1776,-1271.0095,-1272.9766
-1270.6072,-1275.234,-1270.7413,-1276.1057,-1268.2826,-1273.0659,-1270.9648,-1272.9766
-1270.5848,-1275.301,-1270.8083,-1276.0834,-1268.1709,-1273.0883,-1270.8755,-1273.0436
-1270.6295,-1275.4128,-1270.9202,-1276.1729,-1268.2603,-1273.1329,-1270.9202,-1273.0883
-1270.6295,-1275.3458,-1270.8307,-1276.1952,-1268.1709,-1273.0659,-1271.0095,-1273.1329
-1270.6072,-1275.3458,-1270.8083,-1276.1952,-1268.2603,-1272.9989,-1271.0767,-1273.0883
-1270.5178,-1275.4128,-1270.719,-1276.1729,-1268.2156,-1273.0436,-1270.9648,-1272.9766
-1270.5178,-1275.301,-1270.6743,-1276.1057,-1268.1486,-1273.0212,-1270.8307,-1272.9541
-1270.6072,-1275.2563,-1270.7413,-1276.1057,-1268.2156,-1272.9989,-1270.8531,-1273.0659
-1270.6072,-1275.3235,-1270.8083,-1276.1057,-1268.1932,-1273.1776,-1270.8755,-1273.0883
-1270.5178,-1275.3235,-1270.6967,-1276.2175,-1268.2156,-1273.1106,-1270.9425,-1273.0659
-1270.6072,-1275.301,-1270.6743,-1276.1729,-1268.3274,-1273.1106,-1271.0767,-1273.0883
-1270.5178,-1275.234,-1270.8307,-1276.061,-1268.2826,-1273.1329,-1271.0095,-1273.0883
-1270.5402,-1275.301,-1270.7413,-1276.1057,-1268.3497,-1273.0436,-1271.0095,-1273.0883
-1270.6072,-1275.301,-1270.6072,-1276.0834,-1268.2156,-1273.0883,-1271.0767,-1273.0659
-1270.4731,-1275.301,-1270.7413,-1276.0834,-1268.1709,-1273.0212,-1270.8531,-1273.0659