Dear Sirs,
My customer asked us about SCLK/fCLK for Farme-Sync of ADS1178.
There is a description of the following 13 page of the data sheet.
(2) SCLK must be continuously running and limited to ratios of 1, 1/2, 1/4, and 1/8 of fCLK.
On the other hand, there is the following description in the 18 page of the data sheet.
The number of SCLKs within a frame period (FSYNC clock) can be any power of two
ratio of clock cycles (1, 1/2, 1/4, etc.), as long as the number of cycles is sufficient to shift the data output
(4)In addition, on SPI 7 page of the data sheet has the following description.)
For best performance, limit fSCLK/fCLK to ratios of 1, 1/2, 1/4, 1/8, etc.
from all channels within one data frame.
Then Question is SCLK / fCLK in Frmae-Sync format Why "Must"?
What is the difference between SCLK / fCLK notation in SPI and Frame-Sync?
By the way, my customer is using 1/16 in Frame-Sync format.
Best Regards,
Y.Hasebe