Hello.
The datasheet says:
8.6.1.4 Reset Register
The DACx750 reset register is written to at address 0x56. Table 17 provides the description.
Table 17. Reset Register
DATA BIT(S): DB0
NAME: RESET
DEFAULT: 0
DESCRIPTION: Software reset bit. Writing 1 to the bit performs a software reset that resets all registers and the ALARM status to the respective power-on reset default value. After reset completes, the RESET bit clears itself.
Question:
How long does it take to complete the reset after writing 0x01 to the reset register?
Best Regards.