Part Number: PGA411Q1EVM
Hi, I get some issues when i learn using the PGA411-Q1 EVM, expect for your help. as follows:
1、the output pin ORS has no signal
IN the GUI, whether i set the XEXT_AMP 0 or 1, the ORS pin always outputs 1.8; when i set the XEXT_AMP 0,the OEX can output normal sine wave. why?
2、How the PGA411 switch from dignostics to normal
In the GUI,when i set SPIDIAG=1,the PGA411 enters into diagnostics. while i read the DEVSTAT7,i find the device keep dignostics state from then on,it keep dignostics state unless i set DIAGEXIT=1。I am puzzeld ,when the device enters into dignostics state ,and perform over the dignose work, why it doesn't switch to normal state?
3、clock
The OSC reads the EVM ECLKSEL Pin 0V,but the EVM sch diagram show it has a external clok circuit。I am puzzeld the device use which clock on earth, internal or external?
Expect for your reply,thanks!