Other Parts Discussed in Thread: THS4524, OPA2350
Hi,
I have a situation with the ADS1278 where it is likely that the /PWDN pins could be active at 3.3V, and only the 1.8V and 3.3V rails are active. The
3.3V /PWDNx voltage is created by a weak pull-up resistor, so is likely to be 0.1mA maximum. The 5V rail will become active in short order, but
I'm concerned that the part could be damaged during this delay.
Thanks, Dan