Hi all,
I have used ADS124S06 to design RTD temperature measurement. Below is my schematic: When the temp=850C,the resistor of RTD is about 400R. IDAC1 comes out from AIN5, IDAC2 comes out from AIN3, AIN1 and AIN2 are the input. And IDAC from ADS124S06 is 1mA, I have calculated the compliance voltage of IDAC, 0.8(R22)+0.4(RTD)+1.72(R2)+0.4(L1)=3.12 < AVDD-0.6=4.4. But when I use this circuit to measure 400R resistor, the voltage of R2 will be unstable. And the voltage wave of RTD is seen fig.2, it was also unstable. If I remove L2, means I did not use IDAC2, the wave will be normal again. What is more, if I reduce the current of IDAC to 0.5 mA, the wave will be normal again. I cannot find the reason, can anyone give me some advices on it? Thanks a lot.
Fig.1
Fig.2