Hello,
My company has implemented an ADS1247IPW in a circuit with a PT100 RTD. Unfortunately, we are getting widely varying readings on the RTD at various temperatures. I am not the circuit design engineer, and am going through a history of ADC and RTD accuracy analysis that was left behind. Currently I am using the SBAS426H datasheet and the SLAU520A reference design doc to double check numbers and calculations made during the initial analysis. Our RTD only has to function in a temperature range from 0 - 43.3 degrees Celsius, and I have determined from Figure 17 in SBAS426H that the greatest gain error for our application is -0.015%.
My question is this: when using this percentage in the Callendar-Van Dusen equations, do I figure in the negative sign when calculating (for example, in equation 62 in SLAU520A)?
I will look forward to hearing back.
Thank you, Megan