Other Parts Discussed in Thread: TMS320F28377D, , MSP-EXP430F5529LP, ADS1605, REF5020
Hello All,
I want interface ADS1148 with controller TMS320F28377D with the SPI communication. It will be really helpful if I can get the code for that. And is it okay to leave pins IEXC0 and IEXC1 open? And I also wanted to know if I am dealing with 0V-3.3V as operating supply voltage ranges what should I connect to pins REFP0 and REFN0 for AIN0 and AIN1?
Is there any other ADC available which is compatible with same controller and have sampling in MSPS?