Other Parts Discussed in Thread: ADS1115
Hello. I not found in datasheet information about reference voltage long term stability. Please tell me about this.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Yes, yes!!! I understand all this!!! But I dont sure that long-term stability included in these gain error values. Datasheet dont mentioned about long-term stability directly. On the contrary (from datasheet, I marked out suspicious word):
9.3.4 Voltage Reference
The ADS1118 has an integrated voltage reference. An external reference cannot be used with this device. Errors
associated with the initial voltage reference accuracy and the reference drift with temperature are included in the
gain error and gain drift specifications in the Electrical Characteristics.
I dont sure that long-term stability error included to initial voltage reference (and gain) error. Generally, long-term stability described separately.
Even if long-term stability error is included in the gain error, is necessary known long-term stability error value separately (because this is uncalibrated gain error, and initial gain error may be set to zero with calibration).
Ilja,
I wasn't able to find any specific data for the ADS1118, however I did find some for the ADS1115. The ADS1115 is basically the same ADC, but with an I2C interface instead of the SPI interface that the ADS1118 has.
This data shows the change of gain error through a HTOL test. This should mimic a long term aging of the device. This data has a sample size of 116 devices.
Based on the plot, the change in gain error is very small compared to the specification of 0.15%
Joseph Wu