Other Parts Discussed in Thread: DAC8760
I am looking to use both the DAC8750 & DAC8760 to replace AD5420 & AD5422 in 4-20mA applications. In the Analog Devices parts the TUE specification for the external Iset-R is better than the internal Iset-R, and the resistor precision has to be accounted for. For the TI parts the external Iset-R specifications are worse than using the internal Iset-R, and the external Iset-R is glossed over. Is there an assumed precision in your specifications or do I need to account for the external Iset-R which would further reduce the precision of the TI Parts. I currently use a .01% 15K ohm 5 PPM resistor. It appears there is no advantage to using an external Iset-R with the TI parts if I am not using a Hart Net Configuration. Is this correct?