Dear Sir/Ma'am,
I am trying to interface ADS1298 with MCU. I have ADS1298 Evaluation kit which comes with Modular Motherboard from TI.
I am little bit confused about power supply requirement of ADS1298, does it require all power supply variations like 1.8V, 3.3V, and 5V to work properly?
I was going through power supply requirement of ADS1298. In user guide i found below text.
"The ADS1298 can operate in a single supply with +3.0V to +5.0V analog supply (AVDD/AVSS) or bipolar
mode supply (±1.5V to ±2.5V). An additional digital supply of and +1.8V to +3.0V digital supply (DVDD) is
required for operation."
ADS1298 is powered by J5 connector in MMB (schematic mentioned below).
and J5 connected to J4 Connector on ADS1298 Evaluation Kit (Schematic Mentioned Below).
So till my understanding, it uses +5VD, +3.3VD, +1.8VD, AGND pins only. No additional digital supply(because i can see DGND pin is not used).
I am novice with this stuff, I just wanted to clarify if i give 3.3V supply from TI MCU, will it work properly?
Regards
Anurag Tamboli