Hello, all. I am trying to test whether or not my DAC8814 is functioning properly. The precision Op-amps that were used with it were fried due to being supplied with too much power. I am trying to test it in a configuration similar to figure 64 in the datasheet. However, with my precision Op-amps are fried and my precision voltage reference is also likely fried so it is hard for me to set up this configuration to test the DAC. I have access to an arduino microcontroller, an assortment of general purpose Op-amps, resistors, capacitors, inductors, and basic electronic workbench devices. Is there any configuration I can use to test the DAC that only uses general purpose parts?