HI, I'm testing DAC8718.
I got a problem that DAC8718 outputs error after power-on, the error output is zero and the right ourput is -15V. then It always outputs +15V when I try to control it.
The wrong phenomenon is very accidental.
I read the paragraph on Power-on Reset Sequencing on page 44. So I test the power sequence.
CH1 is 5V for DVDD, CH2 is 3.3V for IOVDD, CH3 is +15V for AVDD, CH4 is -15V for AVSS
My schematic as follows:
what should I initialize for DAC8718?
Thanks for reading.