Other Parts Discussed in Thread: MSP430F5529
Hi team,
My customer is using ADS1248 to measure a DC voltage. But we met a strange phenomenon. Please see the details as below.
When the device samples the input, the sample result gradually increased from a smaller value to the actual value. For example, when the input is 1.5V, customer will firstly get a 1.4V sample result. Then the following sample result gradually increases from 1.4V to 1.5V in 5 or 6 seconds. This issue always happens after powering up. When the device operates for a while, the issue is gone. Do you have any comment on this issue?
What’s more, do you have the ADS1248 reference software code so I could ask customer check if this is caused by software. Thanks
Best regards,
Wayne