Other Parts Discussed in Thread: ADS1118, ADS1220, ADS124S08, ADS1248
Hi everybody
Datasheet page 13 / TEMPERATURE SENSOR (ADS1232 only) / ... Typically, the difference in diode voltage is 111.7mV @ 25°C.
My question: how typically is this value? The datasheet creates the impression that this 111.7mV @ 25°C is pretty accurate,
At 28.3°C I measure 118.8mV (equivalent to 43.8°C). The device is following correctly while I increase or decrease the temperatur.
Vref: 4.96V
Do I have somewhere an issue?
Best regards
Mehmet