Other Parts Discussed in Thread: PGA460
Hi Akeem,
I have four questions
1. I need more GPIO so that I want to use pin of Rxd and Txd as GPIO
Can I use these?
2. I want to know that a range between the minimum and maximum was followed by frequency
ex:
frequency 58khz
minimum : 17cm
maximum : 6m
Please give me informations that I hope to include 40Khz
3. Please recommend a frequency of transducer to get a range from 10cm to 3m
4. Is tuning capacitor of C20 of PGA450Q1EVM right?
If I adjusted C20, Can I reduce a time of first peak for 3ms?
Please refer the attached file for first wave
The wave is datapath output
WonGeun,