Other Parts Discussed in Thread: DAC8771
Hi,
on a PCB with current outputs 4....20mA we use the Ti device DAC8760.
Within the scope of an FMEDA, the question arose how the current output of the device behaves if
the SPI communication to the master is interrupted or disturbed.
The SPI bus can be monitored via the 8.3.10 watchdog timer and 8.3.11 frame error checking.
But does a detected SPI bus fault also have access to the output current?
If the current output of the DAC8760 is then permanently at the last value or if it goes to 0mA or into the high-Z state?
0mA would be the safe state, which would be important for us.
Thank all