I am evaluting the ADS1178 for a new design in a timing critical design. The design requires repeatable timing.
I notice there are notes that cast doubt on the channel matching of the devices from part to part (but are "good" within the same part). I also see the group delay of approx. 38 samples.
I should note that general latency is NOT critical, but repeatability of the latency IS, over the life of the product.
I plan to use the device with the frame sync protocol, with external circuitry to timestamp the frame sync signal.
Can these devices be calibrated to sub-sample timing relative to the frame sync pulse? (i.e. can I calibrate the group delay to less than 1 / f data) ? If not, how well could I reasonable calibrate them?
I understand an SAR would be better for this, but you would change your mind once you saw the anti aliasing filter needed for the application!