Welcome to the Precision Data Converters Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".
The code for the ADS1292ECG-FE was written using Code Composer studio 4.0.2. Since then, CCS has been updated and may cause problems for users attempting to compile the existing code. The Steps below should fix the problem -
Setup needed for building the ADS1x9x firmware using the new version of CCS (5.2.0) is as mentioned below (There is only one step needed!)
Project Properties --c/c++ Build -- Predefined Symbols
You will see two pre-define names like “__MSP430F5529__” and “__MSP430F5529” as in Image-1.
Delete the second pre-defined name “__MSP430F5529”, save the settings and build the project as in Image-2