• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Data Converters » All Tags » A/D converters
Share
Data Converters
  • /etc... Data Converters /etc... Data Converters
  • Audio Converters Audio Converters
  • High Speed Data Converters High Speed Data Converters
  • Precision Data Converters Precision Data Converters
  • Video Converters Video Converters

Browse by Tags

Data Converters

Welcome to the Data Converters Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".

Tags
You have subscribed to this tag. To view or manage your tag subscriptions, click here.   Close
You have unsubscribed from this tag. To view or manage your tag subscriptions, click here.   Close
You are currently viewing:
A/D converters
  • 1298
  • 24-bit ADC
  • 24-bit ADC 1278 1271 EVM analog input
  • 24-bit sigma delta ADC
  • adc
  • ADC problem
  • ADC problems
  • ads 1298
  • ADS1115
  • ADS1118
  • ADS1146
  • ADS1211
  • ADS1232
  • ADS1241
  • ADS1248
  • ads1256
  • ADS1258
  • ADS1259
  • ADS1271
  • ads1278
  • ads1298
  • ADS1298ECG-FE
  • ads1299
  • ADS8556
  • DAC
Related Posts
  • Forum Post: ADS1112 scaling error

    Tony Sander Tony Sander
    I am experiencing a severe scaling error with this device. With the PGA set to x8 (256mV FS) I am getting the MSB at 01111111 with ~+182mV input. With the gain reduced to x4 (512mV FS) the MSB hits 01111111 at ~+285mV. Do I have damaged device or is this due to the input circuit impedance?
    on May 20, 2009
  • Forum Post: TVP7002 handling of VGA resolutions coming from component input

    Nir Aloni Nir Aloni
    I currently use the DM6467 EVM which has TVP7002 in its component video input. I noticed that when I connect a source which outputs 800X600@60 resolution to the EVM component input, the TVP7002 identifies this resolution as 720P as indicated by its 'lines per frame' register (lines per frame...
    on Jun 23, 2009
  • Forum Post: ADS1178 EVM IO Voltage

    Rob Mitchell Rob Mitchell
    I am trying to connect the ADS1178 EVM board using 1.8V I/O. The ADS1178 EVM has a 1.8V pin, J3.7, but it does not seem to be going anywhere. Is that correct? Another option is to bypass U16 on the ADS1178EVM and tie DVDD, IOVDD and 1.8V together at J13/J14. If I do this option, it looks like the...
    on Jul 9, 2009
  • Forum Post: ADS1243IPW offset problem in differential mode

    Pang Pang
    Hi all, I am designing a 4 channel differential 4->20mA analog input using the ADS1243I from Texas Instruments. The front end basically consist of resistors network, since we are catering for both voltage input and 4-20mA input using jumpers. The problem comes when the value of some differential...
    on Aug 4, 2009
  • Forum Post: TVP5150AM1 no NTSC colour lock

    David Ambry David Ambry
    Hi there, My TVP5150AM1 application does not colour lock on NTSC, but does on PAL. Luminance is always correctly decoded. Sometimes Pr is correctly decoded, but in that case there is no Pb. Some background information: The device is clocked from the crystal output of a 3.3V 8051-family...
    on Aug 17, 2009
  • Forum Post: ADS1258 problem

    Erwin Saavedra Erwin Saavedra
    hi everyone, i have a problem with reading the ads1258 and i would very much appreciate if anyone can help me. i have it connected to -2.5v and 2.5v (avdd and avss) and to 5v and 0 for the digital interface (basically the same as in the ECG reference). reference voltage is set at 2.5v (and also tested...
    on Dec 14, 2009
  • Forum Post: TVP5150 question

    ZHENGXU HUANG ZHENGXU HUANG
    HI, all I am using TVP5150A connecting with a PAL camera as input, and connect to DM642.The TVP5150 output is a standard ITU-R 8bit BT656 4:2:2 (720*576) with embedded synchronization(SAV and EAV).The DM642 is used to process the BT656 data.ALL function is OK .However the output video has a black...
    on Jan 11, 2010
  • Forum Post: ADS1278 to OMAP3530 via SPI

    John Thomas43830 John Thomas43830
    We are building a connection between the ADS1278 (ADS1278EVM) and the OMAP3530 (Gumstix with PALO43). We will only be using one ADS1278 and therefore there will be no daisy-chaining of A/D devices. Some of the current issues unresolved are the following: 1. ADS1278 has no "chip enable/select"...
    on Feb 27, 2010
  • Forum Post: Re: ADS1298 open source design help request & this will assist open source and development & interest in the chip

    josh wojnas josh wojnas
    any sugjestions or problems with the design you noticed? Any of the ground or power at the wrong value etc?
    on May 3, 2010
  • Forum Post: Re: DDC EVM Channel Differences

    Jason Bridgmon Jason Bridgmon
    Hello Drake, A good test to verify it is not something to do with the input is to put the device into test-mode by setting the TEST pin high and collecting data. If you still see radically different A side-B side matching data, then you can look to the reference or supply or something systemic...
    on May 6, 2010
  • Forum Post: Re: DDC EVM Channel Differences

    Jason Bridgmon Jason Bridgmon
    Drake, We did some ballpark measurements on an EVM for a newer DDC product EVM and found trace capacitance to be from 9pF to 11.5pF. I would expect the DDC114 EVM traces would be similar. There is a document on the DDC112 EVM kit from 2000 that goes into some detail about how to lay out traces...
    on May 6, 2010
  • Forum Post: ADS1271: F_SCLK faster than F_CLK

    Sergio L. Sergio L.
    Hello, We're porting a design from a previous ADS to ADS1271. The system uses the SPI interface to read data with F_SCLK = 15 Mhz, but the conversion clock is set to F_CLK = 300 Khz aprox. This violates the technical specification, which states that fSCLK must be lower or equal than fCLK. We...
    on Jun 1, 2010
  • Forum Post: Noise on ADS1298

    MirkoMitrovic MirkoMitrovic
    Hi, does anyone has experience with p-p noise of ADS1298? In datasheet I found 4uV p-p, and this is quite lot for EEG. Is there any information I've missed? Thanks, Mirko
    on Jun 3, 2010
  • Forum Post: ADS1278 spurious signal

    Roberto Signori Roberto Signori
    I am using an ads1278 for signal acquisition. The device is connected to TMS320F2812 dsp for signal analysis. The problem is that I have always two spurious signals on each channel, different channel for channel, A/D converter to A/D converter. The two spurious signal seems 15 to 20 dB higher than...
    on Jun 4, 2010
  • Forum Post: /DVALID

    Woody Ato Woody Ato
    I use the DCC18 und I want do a daisy-chain with 2 DDC118. I don't know, if it's possible to connect the two (2) /DVALID together. The Data retrieval must be done for 16 sensor simultaneous. Thanks for any input! Arrah
    on Jul 30, 2010
  • Forum Post: Re: /DVALID

    Woody Ato Woody Ato
    Hi Tom, Thanks you for your answer, but I think that AND gate wil perfect. The AND will help me to poll the different DVALID (Dvalid 1 & Dvalid 2). what do you think? Thanks Woody
    on Aug 2, 2010
  • Forum Post: ADS1256 conversion accuracy after self-calibration

    Carsten Gehrke Carsten Gehrke
    My circuit uses an ADS1256 and applies differential signals to 3 of the 4 available pairs. One pair, AIN2 & AIN3, is only connected to test pins. After self-calibration, the ADC reports 3.13 VDC for a 2.996 VDC input signal (as measured with a 6-1/2 digit DMM), for an error of about 5%. If I perform...
    on Aug 20, 2010
  • Forum Post: Re: ADS1256 conversion accuracy after self-calibration

    Carsten Gehrke Carsten Gehrke
    Hello Joseph, I am measuring the output of a power supply (Leader DC Tracking Power Supply LPS151) connected directly to AIN2 and AIN3. The reference voltage of 2.5 V is generated on-board by an ADR421 voltage reference, connected by one each 49.9 ohm resistor from V out to VRFP and GND to VRFN, respectively...
    on Aug 20, 2010
  • Forum Post: Re: ADS1256 conversion accuracy after self-calibration

    Carsten Gehrke Carsten Gehrke
    Hello Joseph, Before I made the recordings I posted earlier, I did measure the output of the voltage reference. It was 2.5000 V. This was also the case after the other measurements. I was not able to measure both the input and reference voltages simultaneously because I only had access to one DMM...
    on Aug 21, 2010
  • Forum Post: Bipolar analog supply design problem for ADS1258

    Xu Linfeng Xu Linfeng
    In our application, the analog inputs are within the -2.5V to +2.5V range. Analog supply +15V, +5V and -15V can be used for the ADC. How to get bipolar ±2.5V supply and reference voltage from the power supply? Industrial (–40°C/105°C) temperature range and low power are required...
    on Oct 13, 2010
  • Forum Post: ads1298 biopotential mesurement chip register configuration questions

    josh wojnas josh wojnas
    ads1298 biopotential mesurement chip register configuration questions: I am setting up the regiserts for the ads1298 & I have made a spread sheet of how I think it should be configured for my experaments. Right now I am looking at regiser 4 write register address 4 LOFF 1:0=10 do not...
    on Oct 14, 2010
  • Forum Post: Timing issue with serial flash programming of MSC1211

    Lee Xie Lee Xie
    Hi, folks, In our system, we use serial flash programming to load firmware hex records into a MSC1211 processor . Is there a timing limitation over the serial upgrade procedure, like baud rate, delay between bytes and delay between hex records? many thanks, Lee
    on Nov 30, 2010
  • Forum Post: Offset Errors and Resolution for Delta-Sigma ADC (16-bit ADS1110)

    Leon Rasberry Leon Rasberry
    I have several questions on the TI ADS1110 ADC: (1) I am trying to determine if negative offset readings for a single channel are typical for the ADS1110 ADC device. The data in Decimal for 5 channels (starting with 1 in our numbering) is given below: Chan1 Chan2 Chan3 Chan4 Chan5 14968 00015...
    on Jan 4, 2011
  • Forum Post: ADS1256 Crystal oscilator start-up problems

    Josko Marasovic Josko Marasovic
    Hello, I'm using the ADS1256 in my design and I have used crystal to generate ADC's clock. I followed recommendations from data sheet and evaluation module for clock generation. I have used 7.68 MHz crystal with same properties and parallel capacitors of 18 pF as like as crystal used in...
    on Jan 17, 2011
  • Forum Post: ADS8332 REF-

    CalvinTai CalvinTai
    On page 11 of the ADS8332 datasheet, it mentioned pin "REF-" should connect to AGND through an individual via on th PCB, while on page 20, it said REF- should not be connected to the AGND pin of the converter, instead the REF- must be connect to ghe analog ground plane with a separate via....
    on Feb 10, 2011
12345
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use