Hi,
I have a customer who really likes the scaling in the 5154A however they have multiple streams and like the 5158 - thay are also interfacing to a DM8168. Are there any plans to improve the scaling options of the 5158 or is there another multi-channel decoder we could look at?
Cheers
Calum
Hello Calum,
The TVP5154A and TVP5158 are the only multi-channel decoders we have in our product line at this time.
Video surveillance applications typically use D1 or 1/2-D1 resolution which both devices support.
What additional scaling options do you require for your application?
Regards,
Jim
Thanks Jim.
The requiremnets from the customer are such that there could be many permutations of sacling. It could be done inside the DM6168 but since we need the decoder externally it would be nice to have all the sacling there.