I got the below question:
WE decided to use TVP5158
The component has JTAG conector and in the EVM D/S they use 14pin header for JTAG,but ther called it "ARM JTAG"
Accordingly I have couple of questions:
Why they call the JTAG header ARM JTAG?and can I use std 14pin jtag h/w we use for our DSP on this device as well?(they are pin to pin)/
If not,what instruction do I have to communicate with this device?
JTAG was not intended to be used with the TVP5158 during normal operation. This was for debug only. I2C should be used for communication during normal operation.
How about boundary scan, is that supported on the TVP5158?