Hello,
In our current product based on DM8148 and TVP5158, we are planning to utilize the TVP5158 in Line-Interleaved 4-Channel D1 format.
We need information on the format of the Super-frame that will be constructed by the TVP5158.
I understand that the for 8-BIT 656 4-Ch Super-Frame, the TVP5158 will insert the EAV, followed by Horz Blanking+SAV+Start Code+Channel Data.
Is there a pictorial representation of how the one frame is completely merged together?
Also, in terms of the total frame size I am assuming that the Super-frame size will be
4+248+4+8+One Channel Line-Data [720 * 32bits]+4 = 3148 bytes
The same repeated 4 times for 4 different channels i.e., 480 *4 = 1920
Is the above calculation right?
Thanks,
Ravindra