Hi!,
I've got a system using a TVP5158. On one board over three (and I think I've seen a second, but I cannot repeat it), the crystal oscillator (27 Mhz, 18 pf , using 27pF capacitors to a 0R to GND and XTAL-REF) is not starting when the TVP5158 has over 40 C of temp. If it started and it becomes hot, it doesn't stop working.
Things I've tried:
- Changing crystal. Nothing changes.
- Retouch solders on pins. Nothing changes.
- 1Mohm in parallel with the crystal. Nothing changes.
- 100 ohm in series with Xtal-out. Nothing changes.
- A 27 Mhz oscillator to Xtal-in. It works even when is hot! But still not oscillating with the crystal only.
- Flexing the board. Nothing changes.
- Rapid changes in temp. Works if cold, doesn't if hot.
Any ideas?
Thanks in advance!!!