Below is the guide of thermal pad of TVP7002 at the data sheet.
Is there more thermal guide information about using TVP7002?
(With 1080p 60fps usage, TVP7002 goes too high temperature.)
Thanks and regards,
Hayden
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Below is the guide of thermal pad of TVP7002 at the data sheet.
Is there more thermal guide information about using TVP7002?
(With 1080p 60fps usage, TVP7002 goes too high temperature.)
Thanks and regards,
Hayden
Hayden,
These numbers only talk about the transfer of heat from the junction through the package. It is still a requirement to remove the heat from the package.
The TVP7002 can burn 1.4W and the customer systems needs to ensure it is able to remove this amount of heat from the system.
BR,
Steve