I am using the TVP7002 as my VGA capture chip feeding the VIP on our DM8168.
We currently have it set-up for 5-wire RGBHV to YPbPr 4:2:2 ES and this works very well.
We now have a requirement to support RGB sync-on-green 3-wire for the same VESA resolutions (primarily XGA and SXGA)
We have the green signal splitting and going through a 1nf to SOGIN and 100nf to GIN_1.
The chip looks like it sees the SOG signal as the Sync Detect Status register (0x14) reads 0x6f.
The CPL and LPF registers however never show correctly. The CPL registers (0x39 - 0x3a) are always 0x1a6, the LPF registers (0x37 - 0x38) are normally 0x000 but sometimes change to random values even if the resolution has not changed.
At no point have I been able to detect a signal correctly.
Attached is the tvp7002.c driver file we are using. Please let me know if there is a specific set of registers I need to configure differently to make RGB SoG work. Am I the only one having this problem?
Thanks,
-Troy
/* Texas Instruments Triple 8-/10-BIT 165-/110-MSPS Video and Graphics * Digitizer with Horizontal PLL registers * * Copyright (C) 2009 Texas Instruments Inc * Author: Santiago Nunez-Corrales <santiago.nunez@ridgerun.com> * * This code is partially based upon the TVP5150 driver * written by Mauro Carvalho Chehab (mchehab@infradead.org), * the TVP514x driver written by Vaibhav Hiremath <hvaibhav@ti.com> * and the TVP7002 driver in the TI LSP 2.10.00.14. Revisions by * Muralidharan Karicheri and Snehaprabha Narnakaje (TI). * * This program is free software; you can redistribute it and/or modify * it under the terms of the GNU General Public License as published by * the Free Software Foundation; either version 2 of the License, or * (at your option) any later version. * * This program is distributed in the hope that it will be useful, * but WITHOUT ANY WARRANTY; without even the implied warranty of * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the * GNU General Public License for more details. * * You should have received a copy of the GNU General Public License * along with this program; if not, write to the Free Software * Foundation, Inc., 675 Mass Ave, Cambridge, MA 02139, USA. */ #include <linux/delay.h> #include <linux/i2c.h> #include <linux/slab.h> #include <linux/videodev2.h> #include <media/tvp7002.h> #include <media/v4l2-device.h> #include <media/v4l2-chip-ident.h> #include <media/v4l2-common.h> #include "tvp7002_reg.h" MODULE_DESCRIPTION("TI TVP7002 Video and Graphics Digitizer driver"); MODULE_AUTHOR("Santiago Nunez-Corrales <santiago.nunez@ridgerun.com>"); MODULE_LICENSE("GPL"); /* Module Name */ #define TVP7002_MODULE_NAME "tvp7002" /* I2C retry attempts */ #define I2C_RETRY_COUNT (5) /* End of registers */ #define TVP7002_EOR 0x5c /* Read write definition for registers */ #define TVP7002_READ 0 #define TVP7002_WRITE 1 #define TVP7002_RESERVED 2 /* Interlaced vs progressive mask and shift */ #define TVP7002_IP_SHIFT 5 #define TVP7002_INPR_MASK (0x01 << TVP7002_IP_SHIFT) /* Shift for CPL and LPF registers */ #define TVP7002_CL_SHIFT 8 #define TVP7002_CL_MASK 0x0f /* Debug functions */ static int debug = 2; module_param(debug, bool, 0644); MODULE_PARM_DESC(debug, "Debug level (0-2)"); /* Structure for register values */ struct i2c_reg_value { u8 reg; u8 value; u8 type; }; /* * Register default values (according to tvp7002 datasheet) * In the case of read-only registers, the value (0xff) is * never written. R/W functionality is controlled by the * writable bit in the register struct definition. */ static const struct i2c_reg_value tvp7002_init_default_original[] = { { TVP7002_CHIP_REV, 0xff, TVP7002_READ }, { TVP7002_HPLL_FDBK_DIV_MSBS, 0x67, TVP7002_WRITE }, { TVP7002_HPLL_FDBK_DIV_LSBS, 0x20, TVP7002_WRITE }, { TVP7002_HPLL_CRTL, 0xa0, TVP7002_WRITE }, { TVP7002_HPLL_PHASE_SEL, 0x80, TVP7002_WRITE }, { TVP7002_CLAMP_START, 0x32, TVP7002_WRITE }, { TVP7002_CLAMP_W, 0x20, TVP7002_WRITE }, { TVP7002_HSYNC_OUT_W, 0x60, TVP7002_WRITE }, { TVP7002_B_FINE_GAIN, 0x00, TVP7002_WRITE }, { TVP7002_G_FINE_GAIN, 0x00, TVP7002_WRITE }, { TVP7002_R_FINE_GAIN, 0x00, TVP7002_WRITE }, { TVP7002_B_FINE_OFF_MSBS, 0x80, TVP7002_WRITE }, { TVP7002_G_FINE_OFF_MSBS, 0x80, TVP7002_WRITE }, { TVP7002_R_FINE_OFF_MSBS, 0x80, TVP7002_WRITE }, { TVP7002_SYNC_CTL_1, 0x20, TVP7002_WRITE }, { TVP7002_HPLL_AND_CLAMP_CTL, 0x2e, TVP7002_WRITE }, { TVP7002_SYNC_ON_G_THRS, 0x5d, TVP7002_WRITE }, { TVP7002_SYNC_SEPARATOR_THRS, 0x47, TVP7002_WRITE }, { TVP7002_HPLL_PRE_COAST, 0x00, TVP7002_WRITE }, { TVP7002_HPLL_POST_COAST, 0x00, TVP7002_WRITE }, { TVP7002_SYNC_DETECT_STAT, 0xff, TVP7002_READ }, { TVP7002_OUT_FORMATTER, 0x47, TVP7002_WRITE }, { TVP7002_MISC_CTL_1, 0x01, TVP7002_WRITE }, { TVP7002_MISC_CTL_2, 0x00, TVP7002_WRITE }, { TVP7002_MISC_CTL_3, 0x01, TVP7002_WRITE }, //{ TVP7002_IN_MUX_SEL_1, 0x00, TVP7002_WRITE }, { TVP7002_IN_MUX_SEL_1, 0xaa, TVP7002_WRITE },//vin 3 { TVP7002_IN_MUX_SEL_2, 0x67, TVP7002_WRITE }, { TVP7002_B_AND_G_COARSE_GAIN, 0x77, TVP7002_WRITE }, { TVP7002_R_COARSE_GAIN, 0x07, TVP7002_WRITE }, { TVP7002_FINE_OFF_LSBS, 0x00, TVP7002_WRITE }, { TVP7002_B_COARSE_OFF, 0x10, TVP7002_WRITE }, { TVP7002_G_COARSE_OFF, 0x10, TVP7002_WRITE }, { TVP7002_R_COARSE_OFF, 0x10, TVP7002_WRITE }, { TVP7002_HSOUT_OUT_START, 0x08, TVP7002_WRITE }, { TVP7002_MISC_CTL_4, 0x00, TVP7002_WRITE }, { TVP7002_B_DGTL_ALC_OUT_LSBS, 0xff, TVP7002_READ }, { TVP7002_G_DGTL_ALC_OUT_LSBS, 0xff, TVP7002_READ }, { TVP7002_R_DGTL_ALC_OUT_LSBS, 0xff, TVP7002_READ }, { TVP7002_AUTO_LVL_CTL_ENABLE, 0x80, TVP7002_WRITE }, { TVP7002_DGTL_ALC_OUT_MSBS, 0xff, TVP7002_READ }, { TVP7002_AUTO_LVL_CTL_FILTER, 0x53, TVP7002_WRITE }, { 0x29, 0x08, TVP7002_RESERVED }, { TVP7002_FINE_CLAMP_CTL, 0x07, TVP7002_WRITE }, /* PWR_CTL is controlled only by the probe and reset functions */ { TVP7002_PWR_CTL, 0x00, TVP7002_RESERVED }, { TVP7002_ADC_SETUP, 0x50, TVP7002_WRITE }, { TVP7002_COARSE_CLAMP_CTL, 0x00, TVP7002_WRITE }, { TVP7002_SOG_CLAMP, 0x80, TVP7002_WRITE }, { TVP7002_RGB_COARSE_CLAMP_CTL, 0x00, TVP7002_WRITE }, { TVP7002_SOG_COARSE_CLAMP_CTL, 0x04, TVP7002_WRITE }, { TVP7002_ALC_PLACEMENT, 0x5a, TVP7002_WRITE }, { 0x32, 0x18, TVP7002_RESERVED }, { 0x33, 0x60, TVP7002_RESERVED }, { TVP7002_MVIS_STRIPPER_W, 0xff, TVP7002_RESERVED }, { TVP7002_VSYNC_ALGN, 0x10, TVP7002_WRITE }, { TVP7002_SYNC_BYPASS, 0x00, TVP7002_WRITE }, { TVP7002_L_FRAME_STAT_LSBS, 0xff, TVP7002_READ }, { TVP7002_L_FRAME_STAT_MSBS, 0xff, TVP7002_READ }, { TVP7002_CLK_L_STAT_LSBS, 0xff, TVP7002_READ }, { TVP7002_CLK_L_STAT_MSBS, 0xff, TVP7002_READ }, { TVP7002_HSYNC_W, 0xff, TVP7002_READ }, { TVP7002_VSYNC_W, 0xff, TVP7002_READ }, { TVP7002_L_LENGTH_TOL, 0x03, TVP7002_WRITE }, { 0x3e, 0x60, TVP7002_RESERVED }, { TVP7002_VIDEO_BWTH_CTL, 0x01, TVP7002_WRITE }, { TVP7002_AVID_START_PIXEL_LSBS, 0x01, TVP7002_WRITE }, { TVP7002_AVID_START_PIXEL_MSBS, 0x2c, TVP7002_WRITE }, { TVP7002_AVID_STOP_PIXEL_LSBS, 0x06, TVP7002_WRITE }, { TVP7002_AVID_STOP_PIXEL_MSBS, 0x2c, TVP7002_WRITE }, { TVP7002_VBLK_F_0_START_L_OFF, 0x05, TVP7002_WRITE }, { TVP7002_VBLK_F_1_START_L_OFF, 0x00, TVP7002_WRITE }, { TVP7002_VBLK_F_0_DURATION, 0x1e, TVP7002_WRITE }, { TVP7002_VBLK_F_1_DURATION, 0x00, TVP7002_WRITE }, { TVP7002_FBIT_F_0_START_L_OFF, 0x00, TVP7002_WRITE }, { TVP7002_FBIT_F_1_START_L_OFF, 0x00, TVP7002_WRITE }, { TVP7002_YUV_Y_G_COEF_LSBS, 0xe3, TVP7002_WRITE }, { TVP7002_YUV_Y_G_COEF_MSBS, 0x16, TVP7002_WRITE }, { TVP7002_YUV_Y_B_COEF_LSBS, 0x4f, TVP7002_WRITE }, { TVP7002_YUV_Y_B_COEF_MSBS, 0x02, TVP7002_WRITE }, { TVP7002_YUV_Y_R_COEF_LSBS, 0xce, TVP7002_WRITE }, { TVP7002_YUV_Y_R_COEF_MSBS, 0x06, TVP7002_WRITE }, { TVP7002_YUV_U_G_COEF_LSBS, 0xab, TVP7002_WRITE }, { TVP7002_YUV_U_G_COEF_MSBS, 0xf3, TVP7002_WRITE }, { TVP7002_YUV_U_B_COEF_LSBS, 0x00, TVP7002_WRITE }, { TVP7002_YUV_U_B_COEF_MSBS, 0x10, TVP7002_WRITE }, { TVP7002_YUV_U_R_COEF_LSBS, 0x55, TVP7002_WRITE }, { TVP7002_YUV_U_R_COEF_MSBS, 0xfc, TVP7002_WRITE }, { TVP7002_YUV_V_G_COEF_LSBS, 0x78, TVP7002_WRITE }, { TVP7002_YUV_V_G_COEF_MSBS, 0xf1, TVP7002_WRITE }, { TVP7002_YUV_V_B_COEF_LSBS, 0x88, TVP7002_WRITE }, { TVP7002_YUV_V_B_COEF_MSBS, 0xfe, TVP7002_WRITE }, { TVP7002_YUV_V_R_COEF_LSBS, 0x00, TVP7002_WRITE }, { TVP7002_YUV_V_R_COEF_MSBS, 0x10, TVP7002_WRITE }, /* This signals end of register values */ { TVP7002_EOR, 0xff, TVP7002_RESERVED } }; /* TVP7002 default settings .inc */ static const struct i2c_reg_value tvp7002_init_default[] = { { TVP7002_CHIP_REV, 0xff, TVP7002_READ }, { TVP7002_HPLL_FDBK_DIV_MSBS, 0x67, TVP7002_WRITE }, { TVP7002_HPLL_FDBK_DIV_LSBS, 0x20, TVP7002_WRITE }, { TVP7002_HPLL_CRTL, 0xa8, TVP7002_WRITE }, { TVP7002_HPLL_PHASE_SEL, 0x80, TVP7002_WRITE }, { TVP7002_CLAMP_START, 0x32, TVP7002_WRITE }, { TVP7002_CLAMP_W, 0x20, TVP7002_WRITE }, { TVP7002_HSYNC_OUT_W, 0x20, TVP7002_WRITE }, { TVP7002_B_FINE_GAIN, 0x00, TVP7002_WRITE }, { TVP7002_G_FINE_GAIN, 0x00, TVP7002_WRITE }, { TVP7002_R_FINE_GAIN, 0x00, TVP7002_WRITE }, { TVP7002_B_FINE_OFF_MSBS, 0x80, TVP7002_WRITE }, { TVP7002_G_FINE_OFF_MSBS, 0x80, TVP7002_WRITE }, { TVP7002_R_FINE_OFF_MSBS, 0x80, TVP7002_WRITE }, { TVP7002_SYNC_CTL_1, 0x5b, TVP7002_WRITE }, { TVP7002_HPLL_AND_CLAMP_CTL, 0x2a, TVP7002_WRITE }, { TVP7002_SYNC_ON_G_THRS, 0x5d, TVP7002_WRITE }, { TVP7002_SYNC_SEPARATOR_THRS, 0x20, TVP7002_WRITE }, { TVP7002_HPLL_PRE_COAST, 0x00, TVP7002_WRITE }, { TVP7002_HPLL_POST_COAST, 0x00, TVP7002_WRITE }, //{ TVP7002_SYNC_DETECT_STAT, 0xff, TVP7002_READ }, { TVP7002_OUT_FORMATTER, 0x04, TVP7002_WRITE }, { TVP7002_MISC_CTL_1, 0x11, TVP7002_WRITE }, { TVP7002_MISC_CTL_2, 0x73, TVP7002_WRITE }, // start off in tri-state { TVP7002_MISC_CTL_3, 0x00, TVP7002_WRITE }, { TVP7002_IN_MUX_SEL_1, 0xaa, TVP7002_WRITE }, { TVP7002_IN_MUX_SEL_2, 0xc2, TVP7002_WRITE }, // external clock { TVP7002_B_AND_G_COARSE_GAIN, 0x77, TVP7002_WRITE }, { TVP7002_R_COARSE_GAIN, 0x07, TVP7002_WRITE }, { TVP7002_FINE_OFF_LSBS, 0x00, TVP7002_WRITE }, { TVP7002_B_COARSE_OFF, 0x10, TVP7002_WRITE }, { TVP7002_G_COARSE_OFF, 0x10, TVP7002_WRITE }, { TVP7002_R_COARSE_OFF, 0x10, TVP7002_WRITE }, { TVP7002_HSOUT_OUT_START, 0x0d, TVP7002_WRITE }, { TVP7002_MISC_CTL_4, 0x08, TVP7002_WRITE }, { TVP7002_AUTO_LVL_CTL_ENABLE, 0x80, TVP7002_WRITE }, { TVP7002_AUTO_LVL_CTL_FILTER, 0x53, TVP7002_WRITE }, { 0x29, 0x08, TVP7002_RESERVED }, { TVP7002_FINE_CLAMP_CTL, 0x03, TVP7002_WRITE }, /* PWR_CTL is controlled only by the probe and reset functions */ { TVP7002_PWR_CTL, 0x00, TVP7002_RESERVED }, { TVP7002_ADC_SETUP, 0x50, TVP7002_WRITE }, { TVP7002_COARSE_CLAMP_CTL, 0x00, TVP7002_WRITE }, { TVP7002_SOG_CLAMP, 0x80, TVP7002_WRITE }, { TVP7002_RGB_COARSE_CLAMP_CTL, 0x0c, TVP7002_WRITE }, { TVP7002_SOG_COARSE_CLAMP_CTL, 0x04, TVP7002_WRITE }, { TVP7002_ALC_PLACEMENT, 0x5a, TVP7002_WRITE }, { TVP7002_MVIS_STRIPPER_W, 0x03, TVP7002_RESERVED }, { TVP7002_VSYNC_ALGN, 0x10, TVP7002_WRITE }, { TVP7002_SYNC_BYPASS, 0x00, TVP7002_WRITE }, { TVP7002_L_LENGTH_TOL, 0x03, TVP7002_WRITE }, { TVP7002_VIDEO_BWTH_CTL, 0x00, TVP7002_WRITE }, { TVP7002_AVID_START_PIXEL_LSBS, 0x2c, TVP7002_WRITE }, { TVP7002_AVID_START_PIXEL_MSBS, 0x01, TVP7002_WRITE }, { TVP7002_AVID_STOP_PIXEL_LSBS, 0x2c, TVP7002_WRITE }, { TVP7002_AVID_STOP_PIXEL_MSBS, 0x06, TVP7002_WRITE }, { TVP7002_VBLK_F_0_START_L_OFF, 0x05, TVP7002_WRITE }, { TVP7002_VBLK_F_1_START_L_OFF, 0x05, TVP7002_WRITE }, { TVP7002_VBLK_F_0_DURATION, 0x1e, TVP7002_WRITE }, { TVP7002_VBLK_F_1_DURATION, 0x1e, TVP7002_WRITE }, { TVP7002_FBIT_F_0_START_L_OFF, 0x00, TVP7002_WRITE }, { TVP7002_FBIT_F_1_START_L_OFF, 0x00, TVP7002_WRITE }, { TVP7002_YUV_Y_G_COEF_LSBS, 0xe3, TVP7002_WRITE }, { TVP7002_YUV_Y_G_COEF_MSBS, 0x16, TVP7002_WRITE }, { TVP7002_YUV_Y_B_COEF_LSBS, 0x4f, TVP7002_WRITE }, { TVP7002_YUV_Y_B_COEF_MSBS, 0x02, TVP7002_WRITE }, { TVP7002_YUV_Y_R_COEF_LSBS, 0xce, TVP7002_WRITE }, { TVP7002_YUV_Y_R_COEF_MSBS, 0x06, TVP7002_WRITE }, { TVP7002_YUV_U_G_COEF_LSBS, 0xab, TVP7002_WRITE }, { TVP7002_YUV_U_G_COEF_MSBS, 0xf3, TVP7002_WRITE }, { TVP7002_YUV_U_B_COEF_LSBS, 0x00, TVP7002_WRITE }, { TVP7002_YUV_U_B_COEF_MSBS, 0x10, TVP7002_WRITE }, { TVP7002_YUV_U_R_COEF_LSBS, 0x55, TVP7002_WRITE }, { TVP7002_YUV_U_R_COEF_MSBS, 0xfc, TVP7002_WRITE }, { TVP7002_YUV_V_G_COEF_LSBS, 0x78, TVP7002_WRITE }, { TVP7002_YUV_V_G_COEF_MSBS, 0xf1, TVP7002_WRITE }, { TVP7002_YUV_V_B_COEF_LSBS, 0x88, TVP7002_WRITE }, { TVP7002_YUV_V_B_COEF_MSBS, 0xfe, TVP7002_WRITE }, { TVP7002_YUV_V_R_COEF_LSBS, 0x00, TVP7002_WRITE }, { TVP7002_YUV_V_R_COEF_MSBS, 0x10, TVP7002_WRITE }, /* This signals end of register values */ { TVP7002_EOR, 0xff, TVP7002_RESERVED } }; /* Register parameters for 480P */ static const struct i2c_reg_value tvp7002_parms_480P[] = { { TVP7002_HPLL_FDBK_DIV_MSBS, 0x35, TVP7002_WRITE }, { TVP7002_HPLL_FDBK_DIV_LSBS, 0xa0, TVP7002_WRITE }, { TVP7002_HPLL_CRTL, 0x02, TVP7002_WRITE }, { TVP7002_HPLL_PHASE_SEL, 0x14, TVP7002_WRITE }, { TVP7002_AVID_START_PIXEL_LSBS, 0x91, TVP7002_WRITE }, { TVP7002_AVID_START_PIXEL_MSBS, 0x00, TVP7002_WRITE }, { TVP7002_AVID_STOP_PIXEL_LSBS, 0x0B, TVP7002_WRITE }, { TVP7002_AVID_STOP_PIXEL_MSBS, 0x00, TVP7002_WRITE }, { TVP7002_VBLK_F_0_START_L_OFF, 0x03, TVP7002_WRITE }, { TVP7002_VBLK_F_1_START_L_OFF, 0x01, TVP7002_WRITE }, { TVP7002_VBLK_F_0_DURATION, 0x13, TVP7002_WRITE }, { TVP7002_VBLK_F_1_DURATION, 0x13, TVP7002_WRITE }, { TVP7002_ALC_PLACEMENT, 0x18, TVP7002_WRITE }, { TVP7002_CLAMP_START, 0x06, TVP7002_WRITE }, { TVP7002_CLAMP_W, 0x10, TVP7002_WRITE }, { TVP7002_HPLL_PRE_COAST, 0x03, TVP7002_WRITE }, { TVP7002_HPLL_POST_COAST, 0x03, TVP7002_WRITE }, { TVP7002_EOR, 0xff, TVP7002_RESERVED } }; /* Common .inc */ static const struct i2c_reg_value tvp7002_parms_vga_input_common[] = { { TVP7002_HPLL_PHASE_SEL, 0x00, TVP7002_WRITE }, { TVP7002_CLAMP_START, 0x06, TVP7002_WRITE }, { TVP7002_CLAMP_W, 0x10, TVP7002_WRITE }, { TVP7002_HPLL_AND_CLAMP_CTL, 0x2e, TVP7002_WRITE }, //{ TVP7002_SYNC_CTL_1, 0x49, TVP7002_WRITE }, { TVP7002_SYNC_ON_G_THRS, 0x58, TVP7002_WRITE }, { TVP7002_SYNC_SEPARATOR_THRS, 0x40, TVP7002_WRITE }, { TVP7002_HPLL_PRE_COAST, 0x01, TVP7002_WRITE }, { TVP7002_HPLL_POST_COAST, 0x00, TVP7002_WRITE }, { TVP7002_IN_MUX_SEL_1, 0x00, TVP7002_WRITE },//CH1 selected { TVP7002_IN_MUX_SEL_2, 0xca, TVP7002_WRITE }, { TVP7002_AUTO_LVL_CTL_ENABLE, 0x80, TVP7002_WRITE }, { TVP7002_AUTO_LVL_CTL_FILTER, 0x53, TVP7002_WRITE }, { TVP7002_FINE_CLAMP_CTL, 0x87, TVP7002_WRITE }, { TVP7002_PWR_CTL, 0x00, TVP7002_WRITE }, { TVP7002_ALC_PLACEMENT, 0x18, TVP7002_WRITE }, { TVP7002_VSYNC_ALGN, 0x00, TVP7002_WRITE }, { TVP7002_SYNC_BYPASS, 0x00, TVP7002_WRITE }, { TVP7002_L_LENGTH_TOL, 0x06, TVP7002_WRITE }, { TVP7002_VIDEO_BWTH_CTL, 0x00, TVP7002_WRITE }, { TVP7002_B_FINE_GAIN, 0x04, TVP7002_WRITE },//for 20-bit YCbCr 4:2:2 output { TVP7002_G_FINE_GAIN, 0x04, TVP7002_WRITE }, { TVP7002_R_FINE_GAIN, 0x04, TVP7002_WRITE }, { TVP7002_B_FINE_OFF_MSBS, 0x90, TVP7002_WRITE }, { TVP7002_G_FINE_OFF_MSBS, 0x90, TVP7002_WRITE }, { TVP7002_R_FINE_OFF_MSBS, 0x90, TVP7002_WRITE }, { TVP7002_OUT_FORMATTER, 0x43, TVP7002_WRITE }, { TVP7002_MISC_CTL_1, 0x11, TVP7002_WRITE }, { TVP7002_MISC_CTL_2, 0x73, TVP7002_WRITE }, // start off in tri-state { TVP7002_MISC_CTL_3, 0x11, TVP7002_WRITE }, { TVP7002_HSOUT_OUT_START, 0x22, TVP7002_WRITE }, { TVP7002_MISC_CTL_4, 0x00, TVP7002_WRITE }, { TVP7002_EOR, 0xff, TVP7002_RESERVED } }; /* Register parameters for 1240x720 according to TI */ static const struct i2c_reg_value tvp7002_parms_720P60_TI[] = { { TVP7002_HPLL_FDBK_DIV_MSBS, 0x67, TVP7002_WRITE }, { TVP7002_HPLL_FDBK_DIV_LSBS, 0x20, TVP7002_WRITE }, { TVP7002_HPLL_CRTL, 0xa0, TVP7002_WRITE }, { TVP7002_HSYNC_OUT_W, 0x28, TVP7002_WRITE }, { TVP7002_SYNC_CTL_1, 0x36, TVP7002_WRITE }, { TVP7002_ADC_SETUP, 0x50, TVP7002_WRITE }, { TVP7002_AVID_START_PIXEL_LSBS, 0x47, TVP7002_WRITE }, { TVP7002_AVID_START_PIXEL_MSBS, 0x01, TVP7002_WRITE }, { TVP7002_AVID_STOP_PIXEL_LSBS, 0x4b, TVP7002_WRITE }, { TVP7002_AVID_STOP_PIXEL_MSBS, 0x06, TVP7002_WRITE }, { TVP7002_VBLK_F_0_START_L_OFF, 0x05, TVP7002_WRITE }, { TVP7002_VBLK_F_1_START_L_OFF, 0x05, TVP7002_WRITE }, { TVP7002_VBLK_F_0_DURATION, 0x1e, TVP7002_WRITE }, { TVP7002_VBLK_F_1_DURATION, 0x1e, TVP7002_WRITE }, { TVP7002_FBIT_F_0_START_L_OFF, 0x00, TVP7002_WRITE }, { TVP7002_FBIT_F_1_START_L_OFF, 0x00, TVP7002_WRITE }, { TVP7002_EOR, 0xff, TVP7002_RESERVED } }; /* Register parameters for 576P */ static const struct i2c_reg_value tvp7002_parms_576P[] = { { TVP7002_HPLL_FDBK_DIV_MSBS, 0x36, TVP7002_WRITE }, { TVP7002_HPLL_FDBK_DIV_LSBS, 0x00, TVP7002_WRITE }, { TVP7002_HPLL_CRTL, 0x18, TVP7002_WRITE }, { TVP7002_HPLL_PHASE_SEL, 0x14, TVP7002_WRITE }, { TVP7002_AVID_START_PIXEL_LSBS, 0x9B, TVP7002_WRITE }, { TVP7002_AVID_START_PIXEL_MSBS, 0x00, TVP7002_WRITE }, { TVP7002_AVID_STOP_PIXEL_LSBS, 0x0F, TVP7002_WRITE }, { TVP7002_AVID_STOP_PIXEL_MSBS, 0x00, TVP7002_WRITE }, { TVP7002_VBLK_F_0_START_L_OFF, 0x00, TVP7002_WRITE }, { TVP7002_VBLK_F_1_START_L_OFF, 0x00, TVP7002_WRITE }, { TVP7002_VBLK_F_0_DURATION, 0x2D, TVP7002_WRITE }, { TVP7002_VBLK_F_1_DURATION, 0x00, TVP7002_WRITE }, { TVP7002_ALC_PLACEMENT, 0x18, TVP7002_WRITE }, { TVP7002_CLAMP_START, 0x06, TVP7002_WRITE }, { TVP7002_CLAMP_W, 0x10, TVP7002_WRITE }, { TVP7002_HPLL_PRE_COAST, 0x03, TVP7002_WRITE }, { TVP7002_HPLL_POST_COAST, 0x03, TVP7002_WRITE }, { TVP7002_EOR, 0xff, TVP7002_RESERVED } }; /* Register parameters for 1080I60 */ static const struct i2c_reg_value tvp7002_parms_1080I60[] = { { TVP7002_HPLL_FDBK_DIV_MSBS, 0x89, TVP7002_WRITE }, { TVP7002_HPLL_FDBK_DIV_LSBS, 0x80, TVP7002_WRITE }, { TVP7002_HPLL_CRTL, 0x98, TVP7002_WRITE }, { TVP7002_HPLL_PHASE_SEL, 0x14, TVP7002_WRITE }, { TVP7002_AVID_START_PIXEL_LSBS, 0x06, TVP7002_WRITE }, { TVP7002_AVID_START_PIXEL_MSBS, 0x01, TVP7002_WRITE }, { TVP7002_AVID_STOP_PIXEL_LSBS, 0x8a, TVP7002_WRITE }, { TVP7002_AVID_STOP_PIXEL_MSBS, 0x08, TVP7002_WRITE }, { TVP7002_VBLK_F_0_START_L_OFF, 0x02, TVP7002_WRITE }, { TVP7002_VBLK_F_1_START_L_OFF, 0x02, TVP7002_WRITE }, { TVP7002_VBLK_F_0_DURATION, 0x16, TVP7002_WRITE }, { TVP7002_VBLK_F_1_DURATION, 0x17, TVP7002_WRITE }, { TVP7002_ALC_PLACEMENT, 0x5a, TVP7002_WRITE }, { TVP7002_CLAMP_START, 0x32, TVP7002_WRITE }, { TVP7002_CLAMP_W, 0x20, TVP7002_WRITE }, { TVP7002_HPLL_PRE_COAST, 0x01, TVP7002_WRITE }, { TVP7002_HPLL_POST_COAST, 0x00, TVP7002_WRITE }, { TVP7002_EOR, 0xff, TVP7002_RESERVED } }; /* Register parameters for 1080P60 */ static const struct i2c_reg_value tvp7002_parms_1080P60[] = { { TVP7002_HPLL_FDBK_DIV_MSBS, 0x89, TVP7002_WRITE }, { TVP7002_HPLL_FDBK_DIV_LSBS, 0x80, TVP7002_WRITE }, { TVP7002_HPLL_CRTL, 0xe0, TVP7002_WRITE }, { TVP7002_HPLL_PHASE_SEL, 0x00, TVP7002_WRITE }, { TVP7002_HSYNC_OUT_W, 0x2c, TVP7002_WRITE }, { TVP7002_SYNC_CTL_1, 0x36, TVP7002_WRITE }, { TVP7002_SYNC_SEPARATOR_THRS, 0x2d, TVP7002_WRITE }, { TVP7002_HPLL_PRE_COAST, 0x01, TVP7002_WRITE }, { TVP7002_HPLL_POST_COAST, 0x00, TVP7002_WRITE }, { TVP7002_OUT_FORMATTER, 0x23, TVP7002_WRITE }, { TVP7002_MISC_CTL_3, 0x10, TVP7002_WRITE }, { TVP7002_ADC_SETUP, 0x80, TVP7002_WRITE }, { TVP7002_MVIS_STRIPPER_W, 0x09, TVP7002_WRITE }, { TVP7002_AVID_START_PIXEL_LSBS, 0x07, TVP7002_WRITE }, { TVP7002_AVID_START_PIXEL_MSBS, 0x01, TVP7002_WRITE }, { TVP7002_AVID_STOP_PIXEL_LSBS, 0x8b, TVP7002_WRITE }, { TVP7002_AVID_STOP_PIXEL_MSBS, 0x08, TVP7002_WRITE }, { TVP7002_VBLK_F_0_START_L_OFF, 0x04, TVP7002_WRITE }, { TVP7002_VBLK_F_1_START_L_OFF, 0x04, TVP7002_WRITE }, { TVP7002_VBLK_F_0_DURATION, 0x2d, TVP7002_WRITE }, { TVP7002_VBLK_F_1_DURATION, 0x2d, TVP7002_WRITE }, { TVP7002_FBIT_F_0_START_L_OFF, 0x00, TVP7002_WRITE }, { TVP7002_FBIT_F_1_START_L_OFF, 0x00, TVP7002_WRITE }, { TVP7002_EOR, 0xff, TVP7002_RESERVED } }; /* Register parameters for 1080I50 */ static const struct i2c_reg_value tvp7002_parms_1080I50[] = { { TVP7002_HPLL_FDBK_DIV_MSBS, 0xa5, TVP7002_WRITE }, { TVP7002_HPLL_FDBK_DIV_LSBS, 0x00, TVP7002_WRITE }, { TVP7002_HPLL_CRTL, 0x98, TVP7002_WRITE }, { TVP7002_HPLL_PHASE_SEL, 0x14, TVP7002_WRITE }, { TVP7002_AVID_START_PIXEL_LSBS, 0x06, TVP7002_WRITE }, { TVP7002_AVID_START_PIXEL_MSBS, 0x01, TVP7002_WRITE }, { TVP7002_AVID_STOP_PIXEL_LSBS, 0x8a, TVP7002_WRITE }, { TVP7002_AVID_STOP_PIXEL_MSBS, 0x08, TVP7002_WRITE }, { TVP7002_VBLK_F_0_START_L_OFF, 0x02, TVP7002_WRITE }, { TVP7002_VBLK_F_1_START_L_OFF, 0x02, TVP7002_WRITE }, { TVP7002_VBLK_F_0_DURATION, 0x16, TVP7002_WRITE }, { TVP7002_VBLK_F_1_DURATION, 0x17, TVP7002_WRITE }, { TVP7002_ALC_PLACEMENT, 0x5a, TVP7002_WRITE }, { TVP7002_CLAMP_START, 0x32, TVP7002_WRITE }, { TVP7002_CLAMP_W, 0x20, TVP7002_WRITE }, { TVP7002_HPLL_PRE_COAST, 0x01, TVP7002_WRITE }, { TVP7002_HPLL_POST_COAST, 0x00, TVP7002_WRITE }, { TVP7002_EOR, 0xff, TVP7002_RESERVED } }; /* Register parameters for 720P60 */ static const struct i2c_reg_value tvp7002_parms_720P60[] = { { TVP7002_HPLL_FDBK_DIV_MSBS, 0x67, TVP7002_WRITE }, { TVP7002_HPLL_FDBK_DIV_LSBS, 0x20, TVP7002_WRITE }, { TVP7002_HPLL_CRTL, 0xa0, TVP7002_WRITE }, { TVP7002_HPLL_PHASE_SEL, 0x00, TVP7002_WRITE }, { TVP7002_HSYNC_OUT_W, 0x28, TVP7002_WRITE }, { TVP7002_SYNC_CTL_1, 0x36, TVP7002_WRITE }, { TVP7002_SYNC_SEPARATOR_THRS, 0x43, TVP7002_WRITE }, { TVP7002_HPLL_PRE_COAST, 0x01, TVP7002_WRITE }, { TVP7002_HPLL_POST_COAST, 0x00, TVP7002_WRITE }, { TVP7002_OUT_FORMATTER, 0x23, TVP7002_WRITE }, { TVP7002_MISC_CTL_3, 0x10, TVP7002_WRITE }, { TVP7002_ADC_SETUP, 0x50, TVP7002_WRITE }, { TVP7002_MVIS_STRIPPER_W, 0x12, TVP7002_WRITE }, { TVP7002_AVID_START_PIXEL_LSBS, 0x47, TVP7002_WRITE }, { TVP7002_AVID_START_PIXEL_MSBS, 0x01, TVP7002_WRITE }, { TVP7002_AVID_STOP_PIXEL_LSBS, 0x4b, TVP7002_WRITE }, { TVP7002_AVID_STOP_PIXEL_MSBS, 0x06, TVP7002_WRITE }, { TVP7002_VBLK_F_0_START_L_OFF, 0x05, TVP7002_WRITE }, { TVP7002_VBLK_F_1_START_L_OFF, 0x05, TVP7002_WRITE }, { TVP7002_VBLK_F_0_DURATION, 0x1e, TVP7002_WRITE }, { TVP7002_VBLK_F_1_DURATION, 0x1e, TVP7002_WRITE }, { TVP7002_FBIT_F_0_START_L_OFF, 0x00, TVP7002_WRITE }, { TVP7002_FBIT_F_1_START_L_OFF, 0x00, TVP7002_WRITE }, { TVP7002_EOR, 0xff, TVP7002_RESERVED } }; /* Register parameters for 640x480 */ static const struct i2c_reg_value tvp7002_parms_640x480[] = { { TVP7002_HPLL_FDBK_DIV_MSBS, 0x32, TVP7002_WRITE }, { TVP7002_HPLL_FDBK_DIV_LSBS, 0x00, TVP7002_WRITE }, { TVP7002_HPLL_CRTL, 0x20, TVP7002_WRITE }, //{ TVP7002_HPLL_PHASE_SEL, 0x00, TVP7002_WRITE }, { TVP7002_HSYNC_OUT_W, 0x60, TVP7002_WRITE }, { TVP7002_SYNC_CTL_1, 0x12, TVP7002_WRITE }, //{ TVP7002_SYNC_SEPARATOR_THRS, 0x40, TVP7002_WRITE }, //{ TVP7002_HPLL_PRE_COAST, 0x01, TVP7002_WRITE }, //{ TVP7002_HPLL_POST_COAST, 0x00, TVP7002_WRITE }, //{ TVP7002_OUT_FORMATTER, 0x23, TVP7002_WRITE }, //{ TVP7002_MISC_CTL_3, 0x10, TVP7002_WRITE }, { TVP7002_ADC_SETUP, 0x50, TVP7002_WRITE }, //{ TVP7002_MVIS_STRIPPER_W, 0x12, TVP7002_WRITE }, { TVP7002_AVID_START_PIXEL_LSBS, 0xaa, TVP7002_WRITE }, { TVP7002_AVID_START_PIXEL_MSBS, 0x00, TVP7002_WRITE }, { TVP7002_AVID_STOP_PIXEL_LSBS, 0x0e, TVP7002_WRITE }, { TVP7002_AVID_STOP_PIXEL_MSBS, 0x00, TVP7002_WRITE }, { TVP7002_VBLK_F_0_START_L_OFF, 0x09, TVP7002_WRITE }, { TVP7002_VBLK_F_1_START_L_OFF, 0x09, TVP7002_WRITE }, { TVP7002_VBLK_F_0_DURATION, 0x2d, TVP7002_WRITE }, { TVP7002_VBLK_F_1_DURATION, 0x2d, TVP7002_WRITE }, //{ TVP7002_FBIT_F_0_START_L_OFF, 0x00, TVP7002_WRITE }, //{ TVP7002_FBIT_F_1_START_L_OFF, 0x00, TVP7002_WRITE }, { TVP7002_EOR, 0xff, TVP7002_RESERVED } }; /* Register parameters for 800x600 */ static const struct i2c_reg_value tvp7002_parms_800x600[] = { { TVP7002_HPLL_FDBK_DIV_MSBS, 0x42, TVP7002_WRITE }, { TVP7002_HPLL_FDBK_DIV_LSBS, 0x00, TVP7002_WRITE }, { TVP7002_HPLL_CRTL, 0x58, TVP7002_WRITE }, //{ TVP7002_HPLL_PHASE_SEL, 0x00, TVP7002_WRITE }, { TVP7002_HSYNC_OUT_W, 0x80, TVP7002_WRITE }, { TVP7002_SYNC_CTL_1, 0x36, TVP7002_WRITE }, //{ TVP7002_SYNC_SEPARATOR_THRS, 0x40, TVP7002_WRITE }, //{ TVP7002_HPLL_PRE_COAST, 0x01, TVP7002_WRITE }, //{ TVP7002_HPLL_POST_COAST, 0x00, TVP7002_WRITE }, //{ TVP7002_OUT_FORMATTER, 0x23, TVP7002_WRITE }, //{ TVP7002_MISC_CTL_3, 0x10, TVP7002_WRITE }, { TVP7002_ADC_SETUP, 0x50, TVP7002_WRITE }, //{ TVP7002_MVIS_STRIPPER_W, 0x12, TVP7002_WRITE }, { TVP7002_AVID_START_PIXEL_LSBS, 0xf2, TVP7002_WRITE }, { TVP7002_AVID_START_PIXEL_MSBS, 0x00, TVP7002_WRITE }, { TVP7002_AVID_STOP_PIXEL_LSBS, 0x16, TVP7002_WRITE }, { TVP7002_AVID_STOP_PIXEL_MSBS, 0x04, TVP7002_WRITE }, { TVP7002_VBLK_F_0_START_L_OFF, 0x01, TVP7002_WRITE }, { TVP7002_VBLK_F_1_START_L_OFF, 0x01, TVP7002_WRITE }, { TVP7002_VBLK_F_0_DURATION, 0x1c, TVP7002_WRITE }, { TVP7002_VBLK_F_1_DURATION, 0x1c, TVP7002_WRITE }, //{ TVP7002_FBIT_F_0_START_L_OFF, 0x00, TVP7002_WRITE }, //{ TVP7002_FBIT_F_1_START_L_OFF, 0x00, TVP7002_WRITE }, { TVP7002_EOR, 0xff, TVP7002_RESERVED } }; /* Register parameters for 1024x768 */ static const struct i2c_reg_value tvp7002_parms_1024x768[] = { { TVP7002_HPLL_FDBK_DIV_MSBS, 0x54, TVP7002_WRITE }, { TVP7002_HPLL_FDBK_DIV_LSBS, 0x00, TVP7002_WRITE }, { TVP7002_HPLL_CRTL, 0x58, TVP7002_WRITE }, //{ TVP7002_HPLL_PHASE_SEL, 0x00, TVP7002_WRITE }, { TVP7002_HSYNC_OUT_W, 0x88, TVP7002_WRITE }, { TVP7002_SYNC_CTL_1, 0x12, TVP7002_WRITE }, //{ TVP7002_SYNC_SEPARATOR_THRS, 0x40, TVP7002_WRITE }, //{ TVP7002_HPLL_PRE_COAST, 0x01, TVP7002_WRITE }, //{ TVP7002_HPLL_POST_COAST, 0x00, TVP7002_WRITE }, //{ TVP7002_OUT_FORMATTER, 0x23, TVP7002_WRITE }, //{ TVP7002_MISC_CTL_3, 0x10, TVP7002_WRITE }, { TVP7002_ADC_SETUP, 0x50, TVP7002_WRITE }, //{ TVP7002_MVIS_STRIPPER_W, 0x12, TVP7002_WRITE }, { TVP7002_AVID_START_PIXEL_LSBS, 0x42, TVP7002_WRITE }, { TVP7002_AVID_START_PIXEL_MSBS, 0x01, TVP7002_WRITE }, { TVP7002_AVID_STOP_PIXEL_LSBS, 0x06, TVP7002_WRITE }, { TVP7002_AVID_STOP_PIXEL_MSBS, 0x00, TVP7002_WRITE }, { TVP7002_VBLK_F_0_START_L_OFF, 0x02, TVP7002_WRITE }, { TVP7002_VBLK_F_1_START_L_OFF, 0x02, TVP7002_WRITE }, { TVP7002_VBLK_F_0_DURATION, 0x26, TVP7002_WRITE }, { TVP7002_VBLK_F_1_DURATION, 0x26, TVP7002_WRITE }, //{ TVP7002_FBIT_F_0_START_L_OFF, 0x00, TVP7002_WRITE }, //{ TVP7002_FBIT_F_1_START_L_OFF, 0x00, TVP7002_WRITE }, { TVP7002_EOR, 0xff, TVP7002_RESERVED } }; /* Register parameters for 1280x1024 */ static const struct i2c_reg_value tvp7002_parms_1280x1024[] = { { TVP7002_HPLL_FDBK_DIV_MSBS, 0x69, TVP7002_WRITE }, { TVP7002_HPLL_FDBK_DIV_LSBS, 0x80, TVP7002_WRITE }, { TVP7002_HPLL_CRTL, 0xa0, TVP7002_WRITE }, { TVP7002_HSYNC_OUT_W, 0x70, TVP7002_WRITE },//0x7e { TVP7002_SYNC_CTL_1, 0x36, TVP7002_WRITE }, { TVP7002_ADC_SETUP, 0x50, TVP7002_WRITE },//0x80 { TVP7002_AVID_START_PIXEL_LSBS, 0x82, TVP7002_WRITE }, { TVP7002_AVID_START_PIXEL_MSBS, 0x01, TVP7002_WRITE }, { TVP7002_AVID_STOP_PIXEL_LSBS, 0x86, TVP7002_WRITE }, { TVP7002_AVID_STOP_PIXEL_MSBS, 0x06, TVP7002_WRITE }, { TVP7002_VBLK_F_0_START_L_OFF, 0x01, TVP7002_WRITE }, { TVP7002_VBLK_F_1_START_L_OFF, 0x01, TVP7002_WRITE }, { TVP7002_VBLK_F_0_DURATION, 0x2A, TVP7002_WRITE }, { TVP7002_VBLK_F_1_DURATION, 0x2A, TVP7002_WRITE }, { TVP7002_EOR, 0xff, TVP7002_RESERVED } }; static const struct i2c_reg_value tvp7002_parms_1280x1024_SOG[] = { { TVP7002_HPLL_FDBK_DIV_MSBS, 0x69, TVP7002_WRITE }, { TVP7002_HPLL_FDBK_DIV_LSBS, 0x80, TVP7002_WRITE }, { TVP7002_HPLL_CRTL, 0xa0, TVP7002_WRITE }, { TVP7002_HSYNC_OUT_W, 0x70, TVP7002_WRITE },//0x7e { TVP7002_SYNC_CTL_1, 0x36, TVP7002_WRITE },//0x49 { TVP7002_ADC_SETUP, 0x50, TVP7002_WRITE },//0x80 { TVP7002_AVID_START_PIXEL_LSBS, 0x82, TVP7002_WRITE }, { TVP7002_AVID_START_PIXEL_MSBS, 0x01, TVP7002_WRITE }, { TVP7002_AVID_STOP_PIXEL_LSBS, 0x86, TVP7002_WRITE }, { TVP7002_AVID_STOP_PIXEL_MSBS, 0x06, TVP7002_WRITE }, { TVP7002_VBLK_F_0_START_L_OFF, 0x01, TVP7002_WRITE }, { TVP7002_VBLK_F_1_START_L_OFF, 0x01, TVP7002_WRITE }, { TVP7002_VBLK_F_0_DURATION, 0x2A, TVP7002_WRITE }, { TVP7002_VBLK_F_1_DURATION, 0x2A, TVP7002_WRITE }, { TVP7002_EOR, 0xff, TVP7002_RESERVED } }; /* Register parameters for 720P50 */ static const struct i2c_reg_value tvp7002_parms_720P50[] = { { TVP7002_HPLL_FDBK_DIV_MSBS, 0x7b, TVP7002_WRITE }, { TVP7002_HPLL_FDBK_DIV_LSBS, 0xc0, TVP7002_WRITE }, { TVP7002_HPLL_CRTL, 0x98, TVP7002_WRITE }, { TVP7002_HPLL_PHASE_SEL, 0x16, TVP7002_WRITE }, { TVP7002_AVID_START_PIXEL_LSBS, 0x47, TVP7002_WRITE }, { TVP7002_AVID_START_PIXEL_MSBS, 0x01, TVP7002_WRITE }, { TVP7002_AVID_STOP_PIXEL_LSBS, 0x4B, TVP7002_WRITE }, { TVP7002_AVID_STOP_PIXEL_MSBS, 0x06, TVP7002_WRITE }, { TVP7002_VBLK_F_0_START_L_OFF, 0x05, TVP7002_WRITE }, { TVP7002_VBLK_F_1_START_L_OFF, 0x00, TVP7002_WRITE }, { TVP7002_VBLK_F_0_DURATION, 0x2D, TVP7002_WRITE }, { TVP7002_VBLK_F_1_DURATION, 0x00, TVP7002_WRITE }, { TVP7002_ALC_PLACEMENT, 0x5a, TVP7002_WRITE }, { TVP7002_CLAMP_START, 0x32, TVP7002_WRITE }, { TVP7002_CLAMP_W, 0x20, TVP7002_WRITE }, { TVP7002_HPLL_PRE_COAST, 0x01, TVP7002_WRITE }, { TVP7002_HPLL_POST_COAST, 0x00, TVP7002_WRITE }, { TVP7002_EOR, 0xff, TVP7002_RESERVED } }; /* Register parameters for 1920x1200 @ 60 */ static const struct i2c_reg_value tvp7002_parms_1920x1200[] = { { TVP7002_HPLL_FDBK_DIV_MSBS, 0x82, TVP7002_WRITE }, { TVP7002_HPLL_FDBK_DIV_LSBS, 0x00, TVP7002_WRITE }, { TVP7002_HPLL_CRTL, 0xE0, TVP7002_WRITE }, { TVP7002_HSYNC_OUT_W, 0x20, TVP7002_WRITE }, { TVP7002_SYNC_CTL_1, 0x32, TVP7002_WRITE }, { TVP7002_ADC_SETUP, 0x80, TVP7002_WRITE }, { TVP7002_AVID_START_PIXEL_LSBS, 0x8A, TVP7002_WRITE }, { TVP7002_AVID_START_PIXEL_MSBS, 0x00, TVP7002_WRITE }, { TVP7002_AVID_STOP_PIXEL_LSBS, 0x0E, TVP7002_WRITE }, { TVP7002_AVID_STOP_PIXEL_MSBS, 0x08, TVP7002_WRITE }, { TVP7002_VBLK_F_0_START_L_OFF, 0x03, TVP7002_WRITE }, { TVP7002_VBLK_F_1_START_L_OFF, 0x03, TVP7002_WRITE }, { TVP7002_VBLK_F_0_DURATION, 0x23, TVP7002_WRITE }, { TVP7002_VBLK_F_1_DURATION, 0x23, TVP7002_WRITE }, { TVP7002_EOR, 0xff, TVP7002_RESERVED } }; /* Preset definition for handling device operation */ struct tvp7002_preset_definition { u32 preset; const struct i2c_reg_value *p_settings; enum v4l2_colorspace color_space; enum v4l2_field scanmode; u16 progressive; u16 lines_per_frame; u16 cpl_min; u16 cpl_max; }; /* Struct list for digital video presets */ static const struct tvp7002_preset_definition tvp7002_presets[] = { { V4L2_DV_720P60, tvp7002_parms_720P60, V4L2_COLORSPACE_REC709, V4L2_FIELD_NONE, 1, 0x2EE, 0xffff, 153 }, { V4L2_DV_640x480, tvp7002_parms_640x480, V4L2_COLORSPACE_REC709, V4L2_FIELD_NONE, 1, 0x20d, 0xffff, 153 }, { V4L2_DV_640x480_75, tvp7002_parms_640x480, V4L2_COLORSPACE_REC709, V4L2_FIELD_NONE, 1, 0x1f4, 0xffff, 153 }, { V4L2_DV_800x600, tvp7002_parms_800x600, V4L2_COLORSPACE_REC709, V4L2_FIELD_NONE, 1, 0x274, 0xffff, 153 }, { V4L2_DV_1024x768, tvp7002_parms_1024x768, V4L2_COLORSPACE_REC709, V4L2_FIELD_NONE, 1, 0x326, 0xffff, 153 }, { V4L2_DV_1024x768_75, tvp7002_parms_1024x768, V4L2_COLORSPACE_REC709, V4L2_FIELD_NONE, 1, 0x320, 0xffff, 153 }, { V4L2_DV_1280x1024, tvp7002_parms_1280x1024, V4L2_COLORSPACE_REC709, V4L2_FIELD_NONE, 1, 0x427, 0xffff, 153 }, { V4L2_DV_1280x1024, tvp7002_parms_1280x1024_SOG, V4L2_COLORSPACE_REC709, V4L2_FIELD_NONE, 1, 0x310, 0xffff, 153 }, { V4L2_DV_1080I60, tvp7002_parms_1080I60, V4L2_COLORSPACE_REC709, V4L2_FIELD_INTERLACED, 0, 0x465, 181, 205 }, { V4L2_DV_1080I50, tvp7002_parms_1080I50, V4L2_COLORSPACE_REC709, V4L2_FIELD_INTERLACED, 0, 0x465, 217, 245 }, { V4L2_DV_720P50, tvp7002_parms_720P50, V4L2_COLORSPACE_REC709, V4L2_FIELD_NONE, 1, 0x2EE, 163, 183 }, { V4L2_DV_1080P60, tvp7002_parms_1080P60, V4L2_COLORSPACE_REC709, V4L2_FIELD_NONE, 1, 0x465, 0xffff, 102 }, { V4L2_DV_480P59_94, tvp7002_parms_480P, V4L2_COLORSPACE_SMPTE170M, V4L2_FIELD_NONE, 1, 0x20D, 0xffff, 0xffff }, { V4L2_DV_576P50, tvp7002_parms_576P, V4L2_COLORSPACE_SMPTE170M, V4L2_FIELD_NONE, 1, 0x271, 0xffff, 0xffff }, { V4L2_DV_1920x1200_60, tvp7002_parms_1920x1200, V4L2_COLORSPACE_SMPTE170M, V4L2_FIELD_NONE, 1, 0x4D3, 0xffff, 0xffff } }; #define NUM_PRESETS ARRAY_SIZE(tvp7002_presets) /* Device definition */ struct tvp7002 { struct v4l2_subdev sd; const struct tvp7002_config *pdata; int ver; int streaming; const struct tvp7002_preset_definition *current_preset; u8 gain; }; /* * to_tvp7002 - Obtain device handler TVP7002 * @sd: ptr to v4l2_subdev struct * * Returns device handler tvp7002. */ static inline struct tvp7002 *to_tvp7002(struct v4l2_subdev *sd) { return container_of(sd, struct tvp7002, sd); } /* * tvp7002_read - Read a value from a register in an TVP7002 * @sd: ptr to v4l2_subdev struct * @addr: TVP7002 register address * @dst: pointer to 8-bit destination * * Returns value read if successful, or non-zero (-1) otherwise. */ static int tvp7002_read(struct v4l2_subdev *sd, u8 addr, u8 *dst) { struct i2c_client *c = v4l2_get_subdevdata(sd); int retry; int error; for (retry = 0; retry < I2C_RETRY_COUNT; retry++) { error = i2c_smbus_read_byte_data(c, addr); if (error >= 0) { *dst = (u8)error; return 0; } msleep_interruptible(10); } v4l2_err(sd, "TVP7002 read error %d\n", error); return error; } /* * tvp7002_read_err() - Read a register value with error code * @sd: pointer to standard V4L2 sub-device structure * @reg: destination register * @val: value to be read * @err: pointer to error value * * Read a value in a register and save error value in pointer. * Also update the register table if successful */ static inline void tvp7002_read_err(struct v4l2_subdev *sd, u8 reg, u8 *dst, int *err) { if (!*err) *err = tvp7002_read(sd, reg, dst); } /* * tvp7002_write() - Write a value to a register in TVP7002 * @sd: ptr to v4l2_subdev struct * @addr: TVP7002 register address * @value: value to be written to the register * * Write a value to a register in an TVP7002 decoder device. * Returns zero if successful, or non-zero otherwise. */ static int tvp7002_write(struct v4l2_subdev *sd, u8 addr, u8 value) { struct i2c_client *c; int retry; int error; c = v4l2_get_subdevdata(sd); for (retry = 0; retry < I2C_RETRY_COUNT; retry++) { error = i2c_smbus_write_byte_data(c, addr, value); if (error >= 0) return 0; v4l2_warn(sd, "Write: retry ... %d\n", retry); msleep_interruptible(10); } v4l2_err(sd, "TVP7002 write error %d\n", error); return error; } /* * tvp7002_write_err() - Write a register value with error code * @sd: pointer to standard V4L2 sub-device structure * @reg: destination register * @val: value to be written * @err: pointer to error value * * Write a value in a register and save error value in pointer. * Also update the register table if successful */ static inline void tvp7002_write_err(struct v4l2_subdev *sd, u8 reg, u8 val, int *err) { if (!*err) *err = tvp7002_write(sd, reg, val); } /* * tvp7002_g_chip_ident() - Get chip identification number * @sd: ptr to v4l2_subdev struct * @chip: ptr to v4l2_dbg_chip_ident struct * * Obtains the chip's identification number. * Returns zero or -EINVAL if read operation fails. */ static int tvp7002_g_chip_ident(struct v4l2_subdev *sd, struct v4l2_dbg_chip_ident *chip) { u8 rev; int error; struct i2c_client *client = v4l2_get_subdevdata(sd); error = tvp7002_read(sd, TVP7002_CHIP_REV, &rev); if (error < 0) return error; return v4l2_chip_ident_i2c_client(client, chip, V4L2_IDENT_TVP7002, rev); } /* * tvp7002_write_inittab() - Write initialization values * @sd: ptr to v4l2_subdev struct * @regs: ptr to i2c_reg_value struct * * Write initialization values. * Returns zero or -EINVAL if read operation fails. */ static int tvp7002_write_inittab(struct v4l2_subdev *sd, const struct i2c_reg_value *regs) { int error = 0; /* Initialize the first (defined) registers */ while (TVP7002_EOR != regs->reg) { if (TVP7002_WRITE == regs->type) tvp7002_write_err(sd, regs->reg, regs->value, &error); regs++; } return error; } /* * tvp7002_s_dv_preset() - Set digital video preset * @sd: ptr to v4l2_subdev struct * @dv_preset: ptr to v4l2_dv_preset struct * * Set the digital video preset for a TVP7002 decoder device. * Returns zero when successful or -EINVAL if register access fails. */ static int tvp7002_s_dv_preset(struct v4l2_subdev *sd, struct v4l2_dv_preset *dv_preset) { struct tvp7002 *device = to_tvp7002(sd); u32 preset; int i; for (i = 0; i < NUM_PRESETS; i++) { preset = tvp7002_presets[i].preset; if (preset == dv_preset->preset) { device->current_preset = &tvp7002_presets[i]; return tvp7002_write_inittab(sd, tvp7002_presets[i].p_settings); } } return -EINVAL; } /* * tvp7002_g_ctrl() - Get a control * @sd: ptr to v4l2_subdev struct * @ctrl: ptr to v4l2_control struct * * Get a control for a TVP7002 decoder device. * Returns zero when successful or -EINVAL if register access fails. */ static int tvp7002_g_ctrl(struct v4l2_subdev *sd, struct v4l2_control *ctrl) { struct tvp7002 *device = to_tvp7002(sd); switch (ctrl->id) { case V4L2_CID_GAIN: ctrl->value = device->gain; return 0; default: return -EINVAL; } } /* * tvp7002_s_ctrl() - Set a control * @sd: ptr to v4l2_subdev struct * @ctrl: ptr to v4l2_control struct * * Set a control in TVP7002 decoder device. * Returns zero when successful or -EINVAL if register access fails. */ static int tvp7002_s_ctrl(struct v4l2_subdev *sd, struct v4l2_control *ctrl) { struct tvp7002 *device = to_tvp7002(sd); int error = 0; switch (ctrl->id) { case V4L2_CID_GAIN: tvp7002_write_err(sd, TVP7002_R_FINE_GAIN, ctrl->value & 0xff, &error); tvp7002_write_err(sd, TVP7002_G_FINE_GAIN, ctrl->value & 0xff, &error); tvp7002_write_err(sd, TVP7002_B_FINE_GAIN, ctrl->value & 0xff, &error); if (error < 0) return error; /* Set only after knowing there is no error */ device->gain = ctrl->value & 0xff; return 0; default: return -EINVAL; } } /* * tvp7002_queryctrl() - Query a control * @sd: ptr to v4l2_subdev struct * @qc: ptr to v4l2_queryctrl struct * * Query a control of a TVP7002 decoder device. * Returns zero when successful or -EINVAL if register read fails. */ static int tvp7002_queryctrl(struct v4l2_subdev *sd, struct v4l2_queryctrl *qc) { switch (qc->id) { case V4L2_CID_GAIN: /* * Gain is supported [0-255, default=0, step=1] */ return v4l2_ctrl_query_fill(qc, 0, 255, 1, 0); default: return -EINVAL; } } /* * tvp7002_mbus_fmt() - V4L2 decoder interface handler for try/s/g_mbus_fmt * @sd: pointer to standard V4L2 sub-device structure * @f: pointer to mediabus format structure * * Negotiate the image capture size and mediabus format. * There is only one possible format, so this single function works for * get, set and try. */ static int tvp7002_mbus_fmt(struct v4l2_subdev *sd, struct v4l2_mbus_framefmt *f) { struct tvp7002 *device = to_tvp7002(sd); struct v4l2_dv_enum_preset e_preset; int error; /* Calculate height and width based on current standard */ error = v4l_fill_dv_preset_info(device->current_preset->preset, &e_preset); if (error) return error; f->width = e_preset.width; f->height = e_preset.height; f->code = V4L2_MBUS_FMT_YUYV10_1X20; f->field = device->current_preset->scanmode; f->colorspace = device->current_preset->color_space; v4l2_dbg(1, debug, sd, "MBUS_FMT: Width - %d, Height - %d", f->width, f->height); return 0; } /* * tvp7002_query_dv_preset() - query DV preset * @sd: pointer to standard V4L2 sub-device structure * @qpreset: standard V4L2 v4l2_dv_preset structure * * Returns the current DV preset by TVP7002. If no active input is * detected, returns -EINVAL */ static int tvp7002_query_dv_preset(struct v4l2_subdev *sd, struct v4l2_dv_preset *qpreset) { const struct tvp7002_preset_definition *presets = tvp7002_presets; struct tvp7002 *device; u8 progressive; u32 lpfr; u32 cpln; int error = 0; u8 lpf_lsb; u8 lpf_msb; u8 cpl_lsb; u8 cpl_msb; int index; device = to_tvp7002(sd); /* Read standards from device registers */ tvp7002_read_err(sd, TVP7002_L_FRAME_STAT_LSBS, &lpf_lsb, &error); tvp7002_read_err(sd, TVP7002_L_FRAME_STAT_MSBS, &lpf_msb, &error); if (error < 0) return error; tvp7002_read_err(sd, TVP7002_CLK_L_STAT_LSBS, &cpl_lsb, &error); tvp7002_read_err(sd, TVP7002_CLK_L_STAT_MSBS, &cpl_msb, &error); if (error < 0) return error; /* Get lines per frame, clocks per line and interlaced/progresive */ lpfr = lpf_lsb | ((TVP7002_CL_MASK & lpf_msb) << TVP7002_CL_SHIFT); cpln = cpl_lsb | ((TVP7002_CL_MASK & cpl_msb) << TVP7002_CL_SHIFT); progressive = (lpf_msb & TVP7002_INPR_MASK) >> TVP7002_IP_SHIFT; /* Do checking of video modes */ for (index = 0; index < NUM_PRESETS; index++, presets++) { v4l2_dbg(1, debug, sd, "Index: %d\nCurrent lpf = %x, Preset lpf = %x\n", index, lpfr, presets->lines_per_frame); if ((lpfr >= (presets->lines_per_frame - 5) && lpfr <= (presets->lines_per_frame + 5)) && progressive == presets->progressive) { v4l2_dbg(1, debug, sd, "Found a match in index %d\n", index); if (presets->cpl_min == 0xffff) break; if (cpln >= presets->cpl_min && cpln <= presets->cpl_max) break; } } v4l2_dbg(1, debug, sd, "data information: lpf = %x, cpl = %x\n", lpfr, cpln); if (index == NUM_PRESETS) { v4l2_dbg(1, debug, sd, "detection failed: lpf = %x, cpl = %x\n", lpfr, cpln); /* Could not detect a signal, so return the 'invalid' preset */ qpreset->preset = V4L2_DV_INVALID; return 0;//tvp7002_log_status(sd); } /* Set values in found preset */ qpreset->preset = presets->preset; /* Update lines per frame and clocks per line info */ v4l2_dbg(1, debug, sd, "detected preset: %d\n", presets->preset); return 0;//tvp7002_log_status(sd); } #ifdef CONFIG_VIDEO_ADV_DEBUG /* * tvp7002_g_register() - Get the value of a register * @sd: ptr to v4l2_subdev struct * @reg: ptr to v4l2_dbg_register struct * * Get the value of a TVP7002 decoder device register. * Returns zero when successful, -EINVAL if register read fails or * access to I2C client fails, -EPERM if the call is not allowed * by diabled CAP_SYS_ADMIN. */ static int tvp7002_g_register(struct v4l2_subdev *sd, struct v4l2_dbg_register *reg) { struct i2c_client *client = v4l2_get_subdevdata(sd); u8 val; int ret; if (!v4l2_chip_match_i2c_client(client, ®->match)) return -EINVAL; if (!capable(CAP_SYS_ADMIN)) return -EPERM; ret = tvp7002_read(sd, reg->reg & 0xff, &val); reg->val = val; return ret; } /* * tvp7002_s_register() - set a control * @sd: ptr to v4l2_subdev struct * @reg: ptr to v4l2_dbg_register struct * * Get the value of a TVP7002 decoder device register. * Returns zero when successful, -EINVAL if register read fails or * -EPERM if call not allowed. */ static int tvp7002_s_register(struct v4l2_subdev *sd, struct v4l2_dbg_register *reg) { struct i2c_client *client = v4l2_get_subdevdata(sd); if (!v4l2_chip_match_i2c_client(client, ®->match)) return -EINVAL; if (!capable(CAP_SYS_ADMIN)) return -EPERM; return tvp7002_write(sd, reg->reg & 0xff, reg->val & 0xff); } #endif /* * tvp7002_enum_mbus_fmt() - Enum supported mediabus formats * @sd: pointer to standard V4L2 sub-device structure * @index: format index * @code: pointer to mediabus format * * Enumerate supported mediabus formats. */ static int tvp7002_enum_mbus_fmt(struct v4l2_subdev *sd, unsigned index, enum v4l2_mbus_pixelcode *code) { /* Check requested format index is within range */ if (index) return -EINVAL; *code = V4L2_MBUS_FMT_YUYV10_1X20; return 0; } /* * tvp7002_s_stream() - V4L2 decoder i/f handler for s_stream * @sd: pointer to standard V4L2 sub-device structure * @enable: streaming enable or disable * * Sets streaming to enable or disable, if possible. */ static int tvp7002_s_stream(struct v4l2_subdev *sd, int enable) { struct tvp7002 *device = to_tvp7002(sd); int error = 0; if (device->streaming == enable) return 0; if (enable) { /* Set output state on (low impedance means stream on) */ error = tvp7002_write(sd, TVP7002_MISC_CTL_2, 0x00); device->streaming = enable; } else { /* Set output state off (high impedance means stream off) */ error = tvp7002_write(sd, TVP7002_MISC_CTL_2, 0x73); if (error) v4l2_dbg(1, debug, sd, "Unable to stop streaming\n"); device->streaming = enable; } return error; } /* * tvp7002_log_status() - Print information about register settings * @sd: ptr to v4l2_subdev struct * * Log register values of a TVP7002 decoder device. * Returns zero or -EINVAL if read operation fails. */ static int tvp7002_log_status(struct v4l2_subdev *sd) { const struct tvp7002_preset_definition *presets = tvp7002_presets; struct tvp7002 *device = to_tvp7002(sd); struct v4l2_dv_enum_preset e_preset; struct v4l2_dv_preset detected; int i; detected.preset = V4L2_DV_INVALID; /* Find my current standard*/ tvp7002_query_dv_preset(sd, &detected); /* Print standard related code values */ for (i = 0; i < NUM_PRESETS; i++, presets++) if (presets->preset == detected.preset) break; if (v4l_fill_dv_preset_info(device->current_preset->preset, &e_preset)) return -EINVAL; v4l2_info(sd, "Selected DV Preset: %s\n", e_preset.name); v4l2_info(sd, " Pixels per line: %u\n", e_preset.width); v4l2_info(sd, " Lines per frame: %u\n\n", e_preset.height); if (i == NUM_PRESETS) { v4l2_info(sd, "Detected DV Preset: None\n"); } else { if (v4l_fill_dv_preset_info(presets->preset, &e_preset)) return -EINVAL; v4l2_info(sd, "Detected DV Preset: %s\n", e_preset.name); v4l2_info(sd, " Pixels per line: %u\n", e_preset.width); v4l2_info(sd, " Lines per frame: %u\n\n", e_preset.height); } v4l2_info(sd, "Streaming enabled: %s\n", device->streaming ? "yes" : "no"); /* Print the current value of the gain control */ v4l2_info(sd, "Gain: %u\n", device->gain); return 0; } /* * tvp7002_enum_dv_presets() - Enum supported digital video formats * @sd: pointer to standard V4L2 sub-device structure * @preset: pointer to format struct * * Enumerate supported digital video formats. */ static int tvp7002_enum_dv_presets(struct v4l2_subdev *sd, struct v4l2_dv_enum_preset *preset) { /* Check requested format index is within range */ if (preset->index >= NUM_PRESETS) return -EINVAL; return v4l_fill_dv_preset_info(tvp7002_presets[preset->index].preset, preset); } /* V4L2 core operation handlers */ static const struct v4l2_subdev_core_ops tvp7002_core_ops = { .g_chip_ident = tvp7002_g_chip_ident, .log_status = tvp7002_log_status, .g_ctrl = tvp7002_g_ctrl, .s_ctrl = tvp7002_s_ctrl, .queryctrl = tvp7002_queryctrl, #ifdef CONFIG_VIDEO_ADV_DEBUG .g_register = tvp7002_g_register, .s_register = tvp7002_s_register, #endif }; /* Specific video subsystem operation handlers */ static const struct v4l2_subdev_video_ops tvp7002_video_ops = { .enum_dv_presets = tvp7002_enum_dv_presets, .s_dv_preset = tvp7002_s_dv_preset, .query_dv_preset = tvp7002_query_dv_preset, .s_stream = tvp7002_s_stream, .g_mbus_fmt = tvp7002_mbus_fmt, .try_mbus_fmt = tvp7002_mbus_fmt, .s_mbus_fmt = tvp7002_mbus_fmt, .enum_mbus_fmt = tvp7002_enum_mbus_fmt, }; /* V4L2 top level operation handlers */ static const struct v4l2_subdev_ops tvp7002_ops = { .core = &tvp7002_core_ops, .video = &tvp7002_video_ops, }; static struct tvp7002 tvp7002_dev = { .streaming = 0, .current_preset = tvp7002_presets, .gain = 0, }; /* * tvp7002_probe - Probe a TVP7002 device * @c: ptr to i2c_client struct * @id: ptr to i2c_device_id struct * * Initialize the TVP7002 device * Returns zero when successful, -EINVAL if register read fails or * -EIO if i2c access is not available. */ static int tvp7002_probe(struct i2c_client *c, const struct i2c_device_id *id) { struct v4l2_subdev *sd; struct tvp7002 *device; struct v4l2_dv_preset preset; int polarity_a; int polarity_b; u8 revision; u8 val; int error; /* Check if the adapter supports the needed features */ if (!i2c_check_functionality(c->adapter, I2C_FUNC_SMBUS_READ_BYTE | I2C_FUNC_SMBUS_WRITE_BYTE_DATA)) return -EIO; if (!c->dev.platform_data) { v4l_err(c, "No platform data!!\n"); return -ENODEV; } device = kmalloc(sizeof(struct tvp7002), GFP_KERNEL); if (!device) return -ENOMEM; *device = tvp7002_dev; sd = &device->sd; device->pdata = c->dev.platform_data; /* Tell v4l2 the device is ready */ v4l2_i2c_subdev_init(sd, c, &tvp7002_ops); v4l_info(c, "tvp7002 found @ 0x%02x (%s)\n", c->addr, c->adapter->name); error = tvp7002_read(sd, TVP7002_CHIP_REV, &revision); if (error < 0) goto found_error; /* Get revision number */ v4l2_info(sd, "Rev. %02x detected.\n", revision); if (revision != 0x02) v4l2_info(sd, "Unknown revision detected.\n"); /* Initializes TVP7002 to its default values */ error = tvp7002_write_inittab(sd, tvp7002_init_default); if (error < 0) goto found_error; /* Write common settings TVP7002 */ error = tvp7002_write_inittab(sd, tvp7002_parms_vga_input_common); if (error < 0) goto found_error; /* Set polarity information after registers have been set */ polarity_a = 0x20 | device->pdata->hs_polarity << 5 | device->pdata->vs_polarity << 2; error = tvp7002_write(sd, TVP7002_SYNC_CTL_1, polarity_a); if (error < 0) goto found_error; polarity_b = device->pdata->fid_polarity << 2 | device->pdata->sog_polarity << 1 | device->pdata->clk_polarity; error = tvp7002_write(sd, TVP7002_MISC_CTL_3, polarity_b); if (error < 0) goto found_error; /*Read Sync Detect Status*/ error = tvp7002_read(sd, TVP7002_SYNC_DETECT_STAT, &val); if (error < 0) goto found_error; v4l2_info(sd, "Sync: %02x detected.\n", val); /* Set registers according to default video mode */ preset.preset = device->current_preset->preset;//V4L2_DV_720P60 error = tvp7002_s_dv_preset(sd, &preset); found_error: if (error < 0) kfree(device); return error; } /* * tvp7002_remove - Remove TVP7002 device support * @c: ptr to i2c_client struct * * Reset the TVP7002 device * Returns zero. */ static int tvp7002_remove(struct i2c_client *c) { struct v4l2_subdev *sd = i2c_get_clientdata(c); struct tvp7002 *device = to_tvp7002(sd); v4l2_dbg(1, debug, sd, "Removing tvp7002 adapter" "on address 0x%x\n", c->addr); v4l2_device_unregister_subdev(sd); kfree(device); return 0; } /* I2C Device ID table */ static const struct i2c_device_id tvp7002_id[] = { { "tvp7002", 0 }, { } }; MODULE_DEVICE_TABLE(i2c, tvp7002_id); /* I2C driver data */ static struct i2c_driver tvp7002_driver = { .driver = { .owner = THIS_MODULE, .name = TVP7002_MODULE_NAME, }, .probe = tvp7002_probe, .remove = tvp7002_remove, .id_table = tvp7002_id, }; /* * tvp7002_init - Initialize driver via I2C interface * * Register the TVP7002 driver. * Return 0 on success or error code on failure. */ static int __init tvp7002_init(void) { return i2c_add_driver(&tvp7002_driver); } /* * tvp7002_exit - Remove driver via I2C interface * * Unregister the TVP7002 driver. * Returns nothing. */ static void __exit tvp7002_exit(void) { i2c_del_driver(&tvp7002_driver); } module_init(tvp7002_init); module_exit(tvp7002_exit);