TVP5158 just have one register to indicate the video format, if I used all 4 channel input, and the video format of each channel are different, for example, Channel 1:NTSC, Channel 2:PAL,etc. What will happen on this register?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TVP5158 just have one register to indicate the video format, if I used all 4 channel input, and the video format of each channel are different, for example, Channel 1:NTSC, Channel 2:PAL,etc. What will happen on this register?
All registers are repeated for each of the 4 cores.
Basically register 0xfe which cores will receive I2C writes and register 0xff controls which core responds to I2C commands.
See section 4 in the datasheet for full details of how to select which of the 4 cores are currently selected.
BR,
Steve