- Datasheet say “The ADC has nine bits of resolution and runs at a nominal speed of 27 MHz. The clock input for the ADC comes from the horizontal PLL”: so I deduce that if the video input is not present the horizontal PLL can not lock so also the 27MHz is not present. Is it true?
- If I set the Power-down mode bit on Operation Mode Control Register “ADCs are turned off and internal clocks are reduced to minimum”: in this situation the 27MHz is switched off?
- The Power-down mode activated with the register has the same effect of the PDN pin?
- It’s possible to stop the main oscillator (the 14.31818MHz external quartz)?
thank you