Hola,
As subject, does TVP5146M2 can support HD 720p /1080i or SD only?Thanks ~
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
SD only. For ED and HD you need to consider the TVP7002.
BR,
Steve
Hola Steve,
Thank you for the prompt reply but TVP7002 is NRND device.
Original, I want to use TVP5158 designed for YPbPr digital output due to our SoC didn't have 720p digital output support.
Can you brief non NRND's device for TV decoder for me?or any new updated on this series. Thank you very so much ~
The TVP5158 does not support YPbPr either. (note YPbPr is the analog standard. YCbCr is the digital notation for the corresponding analog signal)
Additionally the TVP5158 does not support HD formats, only CVBS.
NRND means that there is very limited design support available. The device will still be available for purchase and there are no immediate plans to make it obsolete.
There are no updated devices on the TI roadmap currently.
BR,
Steve
Hola Steve,
Thank you very so much.
We need a solution which like ADV7181D function and it can input YPbPr or CVBS signal and change this analog signal to digital output (for HD).
Does TI have a solution which can replace with ADV7181D?even commercial grade that we can accepted.
We do not have any devices that can accept both CVBS and HD analog signals.
HD signals need to use the TVP7002.
YPbPr ED (Extended Definition, i.e. 480p) is supported by some CVBS capable devices, but not HD. The TVP7002 is the only device which supports HD formats and it does not support CVBS.
BR,
Steve