Hey, I'm having problems with the active video pixel cropping stop registers (13h and 14h) on the TVP5150APBS (ROM Ver 0x03, 0x21). The start registers seem to work as indicated, except that the effect seems multiplied by 2x. If I write a 1 to the start registers (11h and 12h), the active pixels/line decreases by 2 pixels, and if I write a -1 the active pixels/line increase by 2 pixels. However, all is not well with the stop registers and negative values. If I write a 1 to the stop registers the active pixels per line increase by 2, however, if I write a -1 to the stop registers the active pixels/line drop to 772 (nominal is 1440). I've verified this result by looking at the timing of the AVID output and by looking at the input raster detection in my downsteam device. I've looked for a patch already for the TVP5150APBS, but I can't find it if it exists. Is this a known problem with the TVP5150APBS? Is there a solution? I really need to crop some pixels at the end of the line, so I would appreciate help in resolving this. Using a different TI decoder is not an option.
Thanks.