Hi everyone,
I according to the "8637.tvp7002_THS8200_VGA_YPbPr_settings" configuration tvp7002 capture with 1080p,but use different computer as a source of VGA appeared two kinds of circumstances,tvp7002_no.png and tvp7002_yes.png. it didn't pass tvp7002 is normal in the screen.
The register Settings are as follows:
Comparison of the two TXT. Can i solve this problem by configure tvp7002 register ?
tvp7002_yes.txt
read 0x00 0x00 I2C (0x31): 0x49 = 0x02 read tvp7002 parameter I2C (0x5d): 0x01 = 0x89 I2C (0x5d): 0x02 = 0x80 I2C (0x5d): 0x03 = 0xe0 I2C (0x5d): 0x04 = 0x00 I2C (0x5d): 0x05 = 0x06 I2C (0x5d): 0x06 = 0x10 I2C (0x5d): 0x07 = 0x2c I2C (0x5d): 0x0e = 0xc6 I2C (0x5d): 0x0f = 0x2e I2C (0x5d): 0x10 = 0x58 I2C (0x5d): 0x11 = 0x40 I2C (0x5d): 0x12 = 0x01 I2C (0x5d): 0x13 = 0x00 I2C (0x5d): 0x14 = 0xb5 I2C (0x5d): 0x15 = 0x43 I2C (0x5d): 0x16 = 0x11 I2C (0x5d): 0x18 = 0x11 I2C (0x5d): 0x17 = 0x02 I2C (0x5d): 0x19 = 0x00 I2C (0x5d): 0x1a = 0xca I2C (0x5d): 0x1b = 0x77 I2C (0x5d): 0x1c = 0x07 I2C (0x5d): 0x1d = 0x00 I2C (0x5d): 0x1e = 0x10 I2C (0x5d): 0x1f = 0x10 I2C (0x5d): 0x20 = 0x10 I2C (0x5d): 0x21 = 0x22 I2C (0x5d): 0x22 = 0x00 I2C (0x5d): 0x23 = 0x3a I2C (0x5d): 0x24 = 0x30 I2C (0x5d): 0x25 = 0x10 I2C (0x5d): 0x26 = 0x80 I2C (0x5d): 0x27 = 0x2a I2C (0x5d): 0x28 = 0x53 I2C (0x5d): 0x2a = 0x87 I2C (0x5d): 0x2b = 0x40 I2C (0x5d): 0x2c = 0x80 I2C (0x5d): 0x2d = 0x00 I2C (0x5d): 0x2e = 0x80 I2C (0x5d): 0x2f = 0x8c I2C (0x5d): 0x31 = 0x18 I2C (0x5d): 0x35 = 0x00 I2C (0x5d): 0x36 = 0x00 I2C (0x5d): 0x37 = 0x5e I2C (0x5d): 0x38 = 0x24 I2C (0x5d): 0x39 = 0x60 I2C (0x5d): 0x3a = 0x00 I2C (0x5d): 0x3b = 0x58 I2C (0x5d): 0x3c = 0x03 I2C (0x5d): 0x3d = 0x06 I2C (0x5d): 0x3f = 0x00 I2C (0x5d): 0x40 = 0xda I2C (0x5d): 0x41 = 0x00 I2C (0x5d): 0x42 = 0x5e I2C (0x5d): 0x43 = 0x08 I2C (0x5d): 0x44 = 0x04 I2C (0x5d): 0x45 = 0x04 I2C (0x5d): 0x46 = 0x2d I2C (0x5d): 0x47 = 0x2d I2C (0x5d): 0x48 = 0x00 I2C (0x5d): 0x49 = 0x00
tvp7002_no.txt
read 0x00 0x00 I2C (0x31): 0x49 = 0x02 read tvp7002 parameter I2C (0x5d): 0x01 = 0x89 I2C (0x5d): 0x02 = 0x80 I2C (0x5d): 0x03 = 0xe0 I2C (0x5d): 0x04 = 0x00 I2C (0x5d): 0x05 = 0x06 I2C (0x5d): 0x06 = 0x10 I2C (0x5d): 0x07 = 0x2c I2C (0x5d): 0x0e = 0xc6 I2C (0x5d): 0x0f = 0x2e I2C (0x5d): 0x10 = 0x58 I2C (0x5d): 0x11 = 0x40 I2C (0x5d): 0x12 = 0x01 I2C (0x5d): 0x13 = 0x00 I2C (0x5d): 0x14 = 0x95 I2C (0x5d): 0x15 = 0x43 I2C (0x5d): 0x16 = 0x11 I2C (0x5d): 0x18 = 0x11 I2C (0x5d): 0x17 = 0x02 I2C (0x5d): 0x19 = 0x00 I2C (0x5d): 0x1a = 0xca I2C (0x5d): 0x1b = 0x77 I2C (0x5d): 0x1c = 0x07 I2C (0x5d): 0x1d = 0x00 I2C (0x5d): 0x1e = 0x10 I2C (0x5d): 0x1f = 0x10 I2C (0x5d): 0x20 = 0x10 I2C (0x5d): 0x21 = 0x22 I2C (0x5d): 0x22 = 0x00 I2C (0x5d): 0x23 = 0x37 I2C (0x5d): 0x24 = 0x2f I2C (0x5d): 0x25 = 0x0d I2C (0x5d): 0x26 = 0x80 I2C (0x5d): 0x27 = 0x2a I2C (0x5d): 0x28 = 0x53 I2C (0x5d): 0x2a = 0x87 I2C (0x5d): 0x2b = 0x40 I2C (0x5d): 0x2c = 0x80 I2C (0x5d): 0x2d = 0x00 I2C (0x5d): 0x2e = 0x80 I2C (0x5d): 0x2f = 0x8c I2C (0x5d): 0x31 = 0x18 I2C (0x5d): 0x35 = 0x00 I2C (0x5d): 0x36 = 0x00 I2C (0x5d): 0x37 = 0x5e I2C (0x5d): 0x38 = 0x24 I2C (0x5d): 0x39 = 0x60 I2C (0x5d): 0x3a = 0x00 I2C (0x5d): 0x3b = 0x58 I2C (0x5d): 0x3c = 0x03 I2C (0x5d): 0x3d = 0x06 I2C (0x5d): 0x3f = 0x00 I2C (0x5d): 0x40 = 0xda I2C (0x5d): 0x41 = 0x00 I2C (0x5d): 0x42 = 0x5e I2C (0x5d): 0x43 = 0x08 I2C (0x5d): 0x44 = 0x04 I2C (0x5d): 0x45 = 0x04 I2C (0x5d): 0x46 = 0x2d I2C (0x5d): 0x47 = 0x2d I2C (0x5d): 0x48 = 0x00 I2C (0x5d): 0x49 = 0x00