Other Parts Discussed in Thread: TVP5150A
Hello,
Regarding to the monochrome video(CVBS) input with no color burst on TVP5150AM1, my customer is asking some question.
They are using this device for security camera option product.
(Problem)
After the monochrome video(CVBS) with no color burst is input for more than one hour,
When color video (CVBS)format is input as next input, the output does not change to color. (Keep monochrome.)
This problem is happened in market.
So, we have to make solve this problem as soon as possible.
(Question)
(1) According to e2e(below), I guess that the patch code for firmware is needed to solve this problem.
(Patch code version : v04.8C.AA <- It’ OK?)
My understanding is correct?
http://e2e.ti.com/support/data_converters/videoconverters/f/376/p/60318/216178#216178
(2)The patch code is loaded into internal RAM on TVP5150AM1.
So do we need to load every time device power up or recovery from standby mode ?
Regards,
Tao2199